Part Number: TMS320C6657
Hi experts,
Chapter 2.4 of the SPUGZ3A "Keystone Architecture External Memory Interface (EMIF16) User Guide" shows the following:

Q1. It is noted that each of the above two modes can be enabled. In other words, there are actually three modes of operation: We strobe mode, Select Strobe mode, and operation mode with both disabled(Extended Wait Mode?).
This question assumes that there is a third mode of operation in the question above. In Table 5-17 of the TMS320C5557 data sheet, No.4 and No.5 are listed for the CE-OE timing with SS=0 and SS=1, but there is no difference in the values. There are also two types of No.16 and No.17, but there is no difference in the values.
From the EMIF16 User Guide, we understood that the difference in EMIFCE operation as follows:
- In Asynchronous reads in SS Mode in section 2.5.5.1, EMIFCE and EMIFOE are low when Strobe period starts.
- In Asynchronous reads in Chapter 2.5.4.1 (in which both SS Mode and we Mode are disabled), EMIFCE becomes low wQ2hen the Setup period is started.
Q2. Can you tell us the difference in the timing of read and write cycles when SS Mode is enabled and disabled?
Regards,
Hiromu