This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V: Facing issue with devnp-cpsw9g in qnx.

Part Number: DRA829V
Other Parts Discussed in Thread: DRA829

Facing the same issue described in the below thread on custom board based on dra829 and I have already ethernet firmware running on r5f.

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1318670/processor-sdk-j721e-cpsw9g-integration-with-qnx-7-1

  • Hi, Charan,

    Can you tell us what TI SDKs are being used? Pls provide us with the versions of the same?

    Since the ticket mentions "devnp-cpsw9g in qnx," is it a native device or a virtual (thin-client driver) device with EthFW?

    The linked thread ( DRA829V: J721E/DRA829V CPSW9G SGMII link never comes up — PCS LOCK=1 but PAGE_RX=0 even in SERDES loopback ) mentions the issue has been solved, but there is no info on how it was resolved. Please provide full details.

    Thanks.

  • Ok, missed reading that you are using "ethernet firmware on r5f", so I assume you are using both PSDK QNX and PSDK RTOS.. Are the SDK versions of both the same?

    Is the issue reported in the thread  PROCESSOR-SDK-J721E: CPSW9G integration with QNX 7.1 the same?  If yes, can you tell how you are including the devnp driver? Is it part of QNX-IFS, or is it on the mounted file system? Can you share the complete list of file content of QNX_IFS or the file system (whichever is being used)?

    Thanks.

  • Hi Praveen,

    i have now successfully integrated devnp cpsw9g with rtos ethernet firmware.

    My psdk rtos version :ti-processor-sdk-rtos-j721e-evm-08_06_01_03,and psdk qnx :ti-processor-sdk-qnx_j721e_08_06_00_07.

    My questions

    1) How can i enable mac only ports in devnp cpsw9g driver ? I already enabled mac only ports in ethernet firmware.

    2) Can i build devnp cpsw9g driver in QNX momentics ide, if yes, how ?

     because i have win64 QNX SDP on a Windows machine, i don't have QNX SDP Linux host tools.

    below are logs of my testing.(r5f ethernet firmware prints are using main uart which A72 prints)


    => rproc start 2
    => SERDES: Board_serdesCfgSgmii() = 0
    =======================================================
                CPSW Ethernet Firmware 1
    =======================================================

     yyy

     Init Ethernet Fw:

     Init EthFw_initConfigParams

     Init EnetUtils_min
    Warning: Using 6 MAC address(es) from static pool

     Set clk freq to 500MHz

     EthHwInterVlan_setOpenPrms

     Multicast cfg

     initialize Ethfw

     zz

     In EthFw_init fn

     Set VLAN ID

     VLN

     Set Ethfw mode

     port mode

     Enet RM
    ETHFW: Shared multicasts (software fanout):
    ETHFW: Reserved multicasts:
      01:80:c2:00:00:0e
      01:1b:19:00:00:00

     EthFw_initMcm

     Entered ethfw_Initmcm

     Enetmcm_init

     EnetMcm_getCmdIf

     EnetMcm_acquireHandleInfo
    EnetMcm: CPSW_9G on MAIN NAVSS
    Mdio_open: MDIO manual mode enabled
    MDIO: Re-enabled, polling...
    MDIO: poll 0 ALIVE=0x00000007 CTRL=0x410c013f
    MDIO: poll 1 ALIVE=0x00000007 CTRL=0x410c013f
    MDIO: poll 2 ALIVE=0x00000007 CTRL=0x410c013f
    MDIO: poll 3 ALIVE=0x00000007 CTRL=0x410c013f
    MDIO: poll 4 ALIVE=0x00000007 CTRL=0x410c013f
    PHY 0 is alive
    PHY 1 is alive
    PHY 2 is alive
    EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
    EnetPhy_bindDriver: PHY 2: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
    EnetPhy_bindDriver: PHY 1: OUI:080028 Model:24 Ver:00 <-> 'dp83822' : OK

     end of EthFw_initMcm fn

     App utils assert

     EthFw_setAleBcastEntry

     NNN

     JJJ

     print fw versions if OK:

    ETHFW Version   : 0.02.00
    ETHFW Build Date: Apr  6, 2026
    ETHFW Build Time: 19:17:47
    ETHFW Commit SHA:

    Starting lwIP, local interface IP is 192.168.1.200
    Host MAC address: 70:ff:76:1d:92:c2
    [LWIPIF_LWIP] Enet LLD netif initialized successfully
    Added interface 'ti1', IP is 192.168.1.200
    EthFw: TimeSync PTP enabled
    Rx Flow for Software Inter-VLAN Routing is up
    Skipping Ipc_loadResourceTable for QNX (core : mcu2_0) .....
    CpswProxyServer: Virtual port configuration:
      mpu_1_0 <-> Switch port 0: mpu_1_0_ethswitch-device-0
      mcu_2_1 <-> Switch port 1: mcu_2_1_ethswitch-device-1
    CpswProxyServer: initialization completed (core: mcu2_0)
    REMOTE_SERVICE: Init ... !!!
    [IPC] Virtio_kick: Ipc_mailboxSend failed
    REMOTE_SERVICE: Init ... Done !!!





    # slog2info
    Jan 01 05:30:00.038                       random.5                  low*     0  qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
    Jan 01 05:30:00.038                    random.5..0                 slog*   700  Random is using the Fortuna PRNG
    Jan 01 05:30:00.046                       random.5                  low      0  qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
    Jan 01 05:30:00.046                    random.5..0                 slog    700  Selecting timer as an entropy source
    Jan 01 05:30:00.047                    random.5..0                 slog    700  Registered path names
    Jan 01 05:30:00.047                    random.5..0                 slog    700  random: starting resmgr
    Jan 01 05:30:00.048                    random.5..0                 slog    700  random: Daemonizing the process
    Jan 01 05:30:00.057                    tisci_mgr.6                 slog*   130  TI SCI ResMgr for SOC J721E (version=PSDKQNX_08_06_00, date=Tuesday 17 October 2023 09:43:20 PM IST)
    Jan 01 05:30:00.057                    tisci_mgr.6                 slog    130   SYSFW Firmware Version 9.0.6--v09.00.06 (Kool Koala)
    Jan 01 05:30:00.057                    tisci_mgr.6                 slog    130   SYSFW Firmware revision 0x9
    Jan 01 05:30:00.057                    tisci_mgr.6                 slog    130   SYSFW ABI revision 3.1
    Jan 01 05:30:00.061               shmemallocator.7                 slog*   129  TI Shared memory Allocator for SOC J721E (version=PSDKQNX_08_06_00, date=Tuesday 17 October 2023 09:43:20 PM IST)
    Jan 01 05:30:00.062               shmemallocator.7                 slog    129  initSHM:Block[0] @ 0xaa000000 has free-mem = 0x1c00000 - 28 M
    Jan 01 05:30:00.071                    tiipc_mgr.8                 slog*   133  TI IPC ResMgr for SOC J721E (version=PSDKQNX_08_06_00, date=Tuesday 17 October 2023 09:43:20 PM IST)
    Jan 01 05:30:00.071                    tiipc_mgr.8                 slog    133  tiipc-mgr: Starting TI IPC Resmgr
    Jan 01 05:30:00.071                    tiipc_mgr.8                 slog    133  tiipc-mgr: Using VRING base address: 0xaa000000, size:0x1c00000
    Jan 01 05:30:00.099                    tiipc_mgr.8                 slog    133  [IPC]
    Jan 01 05:30:00.099                    tiipc_mgr.8                 slog    133  Mailbox_plugInterrupt: interrupt Number 489, arg 0x8427D180

    Jan 01 05:30:00.128                    tiipc_mgr.8                 slog    133  [IPC]
    Jan 01 05:30:00.128                    tiipc_mgr.8                 slog    133  Mailbox_plugInterrupt: interrupt Number 490, arg 0x8427D320

    Jan 01 05:30:00.156                    tiipc_mgr.8                 slog    133  [IPC]
    Jan 01 05:30:00.156                    tiipc_mgr.8                 slog    133  Mailbox_plugInterrupt: interrupt Number 491, arg 0x8427D4C0

    Jan 01 05:30:00.185                    tiipc_mgr.8                 slog    133  [IPC]
    Jan 01 05:30:00.185                    tiipc_mgr.8                 slog    133  Mailbox_plugInterrupt: interrupt Number 492, arg 0x8427D660

    Jan 01 05:30:00.214                    tiipc_mgr.8                 slog    133  [IPC]
    Jan 01 05:30:00.214                    tiipc_mgr.8                 slog    133  Mailbox_plugInterrupt: interrupt Number 493, arg 0x8427D800

    Jan 01 05:30:00.223                   tiudma_mgr.9                 slog*   131  TI UDMA ResMgr for SOC J721E (version=PSDKQNX_08_06_00, date=Tuesday 17 October 2023 09:43:20 PM IST)
    Jun 19 05:04:53.714          devb_sdmmc_am65x.4110                 slog*  1800  devb-sdmmc-am65x 1.00A (Apr  4 2026 12:08:23)
    Jun 19 05:04:53.715          devb_sdmmc_am65x.4110                 slog      0  libcam.so (Jun 22 2020 21:33:15) bver 7010003
    Jun 19 05:04:53.716          devb_sdmmc_am65x.4110                 slog   1800  sdio_cd:  insertion path 0, cd state 0x1
    Jun 19 05:04:53.721                     iopkt.4111          main_buffer*     0  tcpip starting
    Jun 19 05:04:53.722                     iopkt.4111          main_buffer      0  smmu support is disabled
    Jun 19 05:04:53.724                     iopkt.4111          main_buffer      0  initializing IPsec...
    Jun 19 05:04:53.724                     iopkt.4111          main_buffer      0   done

    Jun 19 05:04:53.724                     iopkt.4111          main_buffer      0  IPsec: Initialized Security Association Processing.

    Jun 19 05:04:53.726                io_usb_otg.4112                 slog*     0  main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d cdns3-xhci ioport=0x6010000,irq=128,iosize=65536,ioport=0x6410000,irq=136,iosize=65536
    Jun 19 05:04:53.727                     iopkt.4111          main_buffer      0  devnp-cpsw2g.so (null)
    Jun 19 05:04:53.728                     iopkt.4111          main_buffer      0  am0

    Jun 19 05:04:53.728              io_pkt_v6_hc.4111                 slog*     0  cpsw_entry:546 Entry -->
    Jun 19 05:04:53.728              io_pkt_v6_hc.4111                 slog      0  cpsw_attach:718 Entry -->
    Jun 19 05:04:53.729              io_pkt_v6_hc.4111                 slog      0  Success - write to MCU_ENET_CTRL - 0x12
    Jun 19 05:04:53.730              io_pkt_v6_hc.4111                 slog      0  Success - write to MCU_ENET_CLKSEL - 0xf00
    Jun 19 05:04:53.733                io_usb_otg.4112                 slog      0  xhci_init: Initialiaing with sever version: 2
    Jun 19 05:04:53.733                io_usb_otg.4112                 slog      0  xhci_controller_init(2661): devu-hcd-cdns3-xhci.so (Jan 20 2022 16:08:39):  args
    Jun 19 05:04:53.733                io_usb_otg.4112                 slog      0  cdns3_usb_port_info(308)[tid:1]: cdns3: chipset j721e xhci_irq=128 serdes_addr=0x5030000
    Jun 19 05:04:53.738                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, Super speed
    Jun 19 05:04:53.738                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8)
    Jun 19 05:04:53.738                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:1]: b:0 devno 0
    Jun 19 05:04:53.738                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
    Jun 19 05:04:53.739                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
    Jun 19 05:04:53.739                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
    Jun 19 05:04:53.739                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
    Jun 19 05:04:53.739                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
    Jun 19 05:04:53.740                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:1]: 1
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800  MMC CID:
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    MID 0x13, OID 0x4e, PNM G1M15L
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    PRV 0x10, PSN 0x27dea1e3, MDT 10-2022
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800  MMC CSD:
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    CSD_STRUCTURE 3, SPEC_VERS 4, CCC 0x8f5
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    TAAC 127, NSAC 1, TRAN_SPEED 50
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    C_SIZE 4095, C_SIZE_MULT 7
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    READ_BL_LEN 9, WRITE_BL_LEN 9
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    ERASE GRP_SIZE 31, GRP_MULT 31, SIZE 0
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    blksz 512, sectors 2097152, dtr 25000000
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800  MMC EXT CSD:
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    DEVICE_TYPE 0x57, EXT_CSD_REV 8
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    SEC_COUNT 62160896, dtr 200000000
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    HC_ERASE_GRP_SIZE 1, HC_WP_GRP_SIZE 16
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    STROBE 0x1, BKOPS_EN 0x2
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800    Driver type: 0x0
    Jun 19 05:04:53.802          devb_sdmmc_am65x.4110                 slog   1800  CFG:  Timing HS200, DTR 200000000, Bus Width 8 bit

    Jun 19 05:04:53.803          devb_sdmmc_am65x.4110                 slog    100  cam-disk.so (Jun 22 2020 21:33:17)
    Jun 19 05:04:53.841                io_usb_otg.4112                 slog      0  xhci_init: Initialiaing with sever version: 2
    Jun 19 05:04:53.841                io_usb_otg.4112                 slog      0  xhci_controller_init(2661): devu-hcd-cdns3-xhci.so (Jan 20 2022 16:08:39):  args
    Jun 19 05:04:53.841                io_usb_otg.4112                 slog      0  cdns3_usb_port_info(308)[tid:1]: cdns3: chipset j721e xhci_irq=136 serdes_addr=0x0
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:1]: busno 1, parent -1, port 0, Super speed
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8)
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:1]: b:1 devno 0
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
    Jun 19 05:04:53.842                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
    Jun 19 05:04:53.843                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 1, devno 0:1)
    Jun 19 05:04:53.843                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
    Jun 19 05:04:53.843                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:1]: 1
    Jun 19 05:04:53.945                io_usb_otg.4112                 slog      0  usbh_timeout_init(203)[tid:1]: Complete
    Jun 19 05:04:53.951          devb_sdmmc_am65x.4110                 slog   1000  fs-qnx6: Allocation strategy 0
    Jun 19 05:04:53.951          devb_sdmmc_am65x.4110                 slog   1000  fs-qnx6: Use btree directory 0
    Jun 19 05:04:53.957          devb_sdmmc_am65x.4110                 slog   1000  fs-qnx6: fs-qnx6: trim (0,1048576,2) was not requested, but is supported
    Jun 19 05:04:53.980                    qconn.12308                 slog*     0  Couldn't initialize listen service: tcp (Invalid argument)

    Jun 19 05:04:54.008                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 0, portno 1)
    Jun 19 05:04:54.008                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.008                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 0, portno 2)
    Jun 19 05:04:54.008                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.016                io_usb_otg.4112                 slog      0  evt_handler: spurious event
    Jun 19 05:04:54.016                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 1, pdevno 0, portno 1)
    Jun 19 05:04:54.016                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.016                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 1, pdevno 0, portno 2)
    Jun 19 05:04:54.017                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.032                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 0, portno 1)
    Jun 19 05:04:54.032                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.290                io_usb_otg.4112                 slog      0  xhci_get_root_device_speed: port 0 is HIGH speed, psts e03
    Jun 19 05:04:54.290                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 0, port 1, High speed
    Jun 19 05:04:54.290                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d0587c0
    Jun 19 05:04:54.297                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:54.297                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 1
    Jun 19 05:04:54.297                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 1
    Jun 19 05:04:54.318                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:54.318                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:54.318                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 41)
    Jun 19 05:04:54.319                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0451, did 0x8142 enumerated(busno 0, devno 1:2)
    Jun 19 05:04:54.319                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:8]: bdentry 1, dentry 1 0
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058950
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:2]: 1
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog      0  process_xfer_complete: No Outstanding Transfer, slotid = 1 devaddr = 0x1 epnum = 0x1 epdir = 0x80 xring->enq_idx = 0 xring->deq_idx = 0
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog      0  process_xfer_complete: evt->w0 = 0x80073000 evt->w1 = 0x0 evt->w2 = 0x1b000000 evt->w3 = 0x1038001
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog     16  hub_notification_disable(353)[tid:2]:
    Jun 19 05:04:54.320                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058950
    Jun 19 05:04:54.422                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 1, portno 1)
    Jun 19 05:04:54.422                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.650                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 1, port 1, High speed
    Jun 19 05:04:54.650                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d0589a0
    Jun 19 05:04:54.657                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:54.657                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 2
    Jun 19 05:04:54.657                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 2
    Jun 19 05:04:54.678                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:54.678                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:54.678                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 41)
    Jun 19 05:04:54.679                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0x9514 enumerated(busno 0, devno 2:3)
    Jun 19 05:04:54.679                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:8]: bdentry 2, dentry 2 0
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058b30
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:2]: 1
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog      0  process_xfer_complete: No Outstanding Transfer, slotid = 2 devaddr = 0x2 epnum = 0x1 epdir = 0x80 xring->enq_idx = 0 xring->deq_idx = 0
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog      0  process_xfer_complete: evt->w0 = 0x80077000 evt->w1 = 0x0 evt->w2 = 0x1b000000 evt->w3 = 0x2038001
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog     16  hub_notification_disable(353)[tid:2]:
    Jun 19 05:04:54.680                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058b30
    Jun 19 05:04:54.782                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 1, portno 2)
    Jun 19 05:04:54.782                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:54.782                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 1, portno 3)
    Jun 19 05:04:54.782                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.010                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 1, port 3, High speed
    Jun 19 05:04:55.010                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058b80
    Jun 19 05:04:55.017                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:55.017                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 3
    Jun 19 05:04:55.017                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 3
    Jun 19 05:04:55.038                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:55.038                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:55.038                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 41)
    Jun 19 05:04:55.039                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0x9514 enumerated(busno 0, devno 3:4)
    Jun 19 05:04:55.039                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:8]: bdentry 3, dentry 3 0
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058d10
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:2]: 1
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog      0  process_xfer_complete: No Outstanding Transfer, slotid = 3 devaddr = 0x3 epnum = 0x1 epdir = 0x80 xring->enq_idx = 0 xring->deq_idx = 0
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog      0  process_xfer_complete: evt->w0 = 0x8007b000 evt->w1 = 0x0 evt->w2 = 0x1b000000 evt->w3 = 0x3038001
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog     16  hub_notification_disable(353)[tid:2]:
    Jun 19 05:04:55.040                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058d10
    Jun 19 05:04:55.142                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 1, portno 4)
    Jun 19 05:04:55.142                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.370                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 1, port 4, High speed
    Jun 19 05:04:55.370                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058d60
    Jun 19 05:04:55.377                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:55.377                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 4
    Jun 19 05:04:55.377                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 4
    Jun 19 05:04:55.398                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:55.398                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:55.398                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 41)
    Jun 19 05:04:55.399                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0x9514 enumerated(busno 0, devno 4:5)
    Jun 19 05:04:55.399                io_usb_otg.4112                 slog     11  hub_state_inserted(569)[tid:8]: bdentry 4, dentry 4 0
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058ef0
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog     13  hub_configuration_enable(263)[tid:2]: 1
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog      0  process_xfer_complete: No Outstanding Transfer, slotid = 4 devaddr = 0x4 epnum = 0x1 epdir = 0x80 xring->enq_idx = 0 xring->deq_idx = 0
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog      0  process_xfer_complete: evt->w0 = 0x8007f000 evt->w1 = 0x0 evt->w2 = 0x1b000000 evt->w3 = 0x4038001
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog     16  hub_notification_disable(353)[tid:2]:
    Jun 19 05:04:55.400                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058ef0
    Jun 19 05:04:55.502                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 2, portno 1)
    Jun 19 05:04:55.502                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.730                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 2, port 1, High speed
    Jun 19 05:04:55.730                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d058f40
    Jun 19 05:04:55.737                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:55.737                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 5
    Jun 19 05:04:55.737                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 5
    Jun 19 05:04:55.758                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:55.758                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:55.758                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 39)
    Jun 19 05:04:55.759                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0xec00 enumerated(busno 0, devno 5:6)
    Jun 19 05:04:55.761                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128180
    Jun 19 05:04:55.762                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d1281d0
    Jun 19 05:04:55.762                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128220
    Jun 19 05:04:55.762                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 2, portno 2)
    Jun 19 05:04:55.762                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 2, portno 3)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 2, portno 4)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 2, portno 5)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 3, portno 1)
    Jun 19 05:04:55.763                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:55.991                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 3, port 1, High speed
    Jun 19 05:04:55.991                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128270
    Jun 19 05:04:55.998                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:55.998                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 6
    Jun 19 05:04:55.998                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 6
    Jun 19 05:04:56.019                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:56.019                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:56.019                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 39)
    Jun 19 05:04:56.020                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0xec00 enumerated(busno 0, devno 6:7)
    Jun 19 05:04:56.022                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128400
    Jun 19 05:04:56.023                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128450
    Jun 19 05:04:56.023                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d1284a0
    Jun 19 05:04:56.023                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 3, portno 2)
    Jun 19 05:04:56.023                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 3, portno 3)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 3, portno 4)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 3, portno 5)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 4, portno 1)
    Jun 19 05:04:56.024                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.252                io_usb_otg.4112                 slog      8  usb_enum_port(94)[tid:8]: busno 0, parent 4, port 1, High speed
    Jun 19 05:04:56.252                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d1284f0
    Jun 19 05:04:56.259                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 8)
    Jun 19 05:04:56.259                io_usb_otg.4112                 slog     12  usb_device_set_address(245)[tid:8]: b:0 devno 7
    Jun 19 05:04:56.259                io_usb_otg.4112                 slog      0  xHCI: Internal Device Addr 7
    Jun 19 05:04:56.280                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 1, index 0, length 18)
    Jun 19 05:04:56.280                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 9)
    Jun 19 05:04:56.280                io_usb_otg.4112                 slog     11  usb_client_descriptor_get(198)[tid:8]: (type 2, index 0, length 39)
    Jun 19 05:04:56.281                io_usb_otg.4112                 slog      8  usb_enum_port(141)[tid:8]: vid 0x0424, did 0xec00 enumerated(busno 0, devno 7:8)
    Jun 19 05:04:56.283                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128680
    Jun 19 05:04:56.284                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d1286d0
    Jun 19 05:04:56.284                io_usb_otg.4112                 slog      0  xring_create: ep->mbuf = 0x5d128720
    Jun 19 05:04:56.284                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 4, portno 2)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 4, portno 3)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 4, portno 4)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 4, portno 5)
    Jun 19 05:04:56.285                io_usb_otg.4112                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
    Jun 19 05:05:08.297                   iopkt.151567          main_buffer*     0  tcpip starting
    Jun 19 05:05:08.297                   iopkt.151567          main_buffer      0  smmu support is disabled
    Jun 19 05:05:08.299                   iopkt.151567          main_buffer      0  initializing IPsec...
    Jun 19 05:05:08.299                   iopkt.151567          main_buffer      0   done

    Jun 19 05:05:08.299                   iopkt.151567          main_buffer      0  IPsec: Initialized Security Association Processing.

    Jun 19 05:05:08.313                   iopkt.151567          main_buffer      0  devnp-cpsw9g.so (null)
    Jun 19 05:05:08.313                   iopkt.151567          main_buffer      0  an0

    Jun 19 05:05:08.313            io_pkt_v6_hc.151567                 slog*     0  cpsw_entry:546 Entry -->
    Jun 19 05:05:08.313            io_pkt_v6_hc.151567                 slog      0  cpsw_attach:718 Entry -->
    Jun 19 05:05:08.315            io_pkt_v6_hc.151567                 slog      0  CPSW9G Client (core : mpu1_0) .....

    Jun 19 05:05:08.318            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceInitFn(5) has started!
    Jun 19 05:05:08.320            io_pkt_v6_hc.151567                 slog      0  Remote device (core : mpu1_0) .....

    Jun 19 05:05:08.320            io_pkt_v6_hc.151567                 slog      0  Remote Device Framework Endpoint located. Remote Core Id:3, Remote End Point:26

    Jun 19 05:05:08.320            io_pkt_v6_hc.151567                 slog      0  CpswProxy_notifyServiceTskFxn(6) has started!
    Jun 19 05:05:08.321            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceDiscoverTaskFn(7) has started!
    Jun 19 05:05:08.321            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceRxTaskFn(8) has started!
    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceInitFn(5) exited!
    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceTxTaskFn(9) has started!
    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  CpswProxy_rdevCmdTskFxn(10) has started!
    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  Connecting to 'mpu_1_0_ethswitch-device-0'

    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  Registered a device name = mpu_1_0_ethswitch-device-0, id = 0, type = 3

    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  ETHFW Version: 0. 2. 0

    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  ETHFW Build Date (YYYY/MMM/DD):2026/Apr/ 6

    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  ETHFW Commit SHA:
    Jun 19 05:05:08.323            io_pkt_v6_hc.151567                 slog      0  ETHFW PermissionFlag:0x3fffffff, UART Connected:true,UART Id:2
    Jun 19 05:05:08.325            io_pkt_v6_hc.151567                 slog      0  CPSW9G: Attach to CpswProxy Server.

    Jun 19 05:05:08.325            io_pkt_v6_hc.151567                 slog      0  appRemoteDeviceDiscoverTaskFn(7) exited!
    Jun 19 05:05:08.387            io_pkt_v6_hc.151567                 slog      0  Function:CpswProxy_cmdHandler,Handle:a2ba239c,CoreKey:38acb7e6, RxMtu:1522, TxMtu:2024:2024:2024:2024:2024:2024:2024:2024, TxCsum:enabled, MacOnly:0

    Jun 19 05:05:08.387            io_pkt_v6_hc.151567                 slog      0  EnetIf_RemoteAttach:371 RX MTU returned - 1522
    Jun 19 05:05:08.473            io_pkt_v6_hc.151567                 slog      0  Function:CpswProxy_cmdHandler,mac_address:70:ff:76:1d:92:c1

    Jun 19 05:05:08.473            io_pkt_v6_hc.151567                 slog      0  MAC Address: 70:ff:76:1d:92:c1

    # ifconfig
    lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
            inet 127.0.0.1 netmask 0xff000000
            inet6 ::1 prefixlen 128
            inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
    an0: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
            address: 70:ff:76:1d:92:c1
            media: Ethernet none (none full-duplex)
            status: no carrier
    # ifconfig ano 10.10.1.5/16
    ifconfig: SIOCGIFFLAGS ano: No such device or address
    # ifconfig
    lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> mtu 33136
            inet 127.0.0.1 netmask 0xff000000
            inet6 ::1 prefixlen 128
            inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1
    an0: flags=8802<BROADCAST,SIMPLEX,MULTICAST> mtu 1500
            address: 70:ff:76:1d:92:c1
            media: Ethernet none (none full-duplex)
            status: no carrier
    # ifconfig an0 10.10.1.5/16
    Function:CpswProxyServer_allocTxHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6
    Function:CpswProxyServer_allocRxHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010401,InArgsLen:0, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010201,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c1, FlowIdx:172, FlowIdxOffset:0
    Cpsw_ioctlInternal: CPSW: Registered MAC address. ALE entry:12, Policer Entry:3
    Function:CpswProxyServer_registerIpv4MacHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c1 IPv4Addr:10.10.1.5

     SNo.      IP Address          MAC Address
    ------    -------------     -----------------
      1       10.10.1.5     70:ff:76:1d:92:c1
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010224,InArgsLen:132, OutArgsLen:0
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010224,InArgsLen:132, OutArgsLen:0
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010224,InArgsLen:132, OutArgsLen:0
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010222,InArgsLen:144, OutArgsLen:36
    Function:CpswProxyServer_ioctlHandlerCb,HostId:0,Handle:a2ba239c,CoreKey:38acb7e6, Cmd:1010202,InArgsLen:24, OutArgsLen:4
    #

  • Hi Charan,

    First, as noted in the past threads, the SDK 8.06 is more than 3 years old and is outside our standard support. So there would be only limited, best-effort support.

    Now coming to your queries:

    1) How can i enable mac only ports in devnp cpsw9g driver ? I already enabled mac only ports in ethernet firmware.

    Suggest looking at the https://software-dl.ti.com/jacinto7/esd/processor-sdk-qnx-jacinto7/08_06_00_07/exports/docs/qnx_sdk_components_j721e.html#usage-of-devnp-cpsw9g-so documentation. To enable mac-only support, you must be using the command-line options: mac-to-mac=1

    2) Can i build devnp cpsw9g driver in QNX momentics ide, if yes, how ?

    The SDK does not support this. We must follow the command-line build process described in the documentation. https://software-dl.ti.com/jacinto7/esd/processor-sdk-qnx-jacinto7/08_06_00_07/exports/docs/build_steps_j721e.html 

    Note that we have not verified our build on a Windows environment. Suggest running Linux using VMware, VirtualBox, or a similar tool for your builds.

    Thanks.