Part Number: AM5728
Hi TI Team,
I am working with the AM5728 using Processor SDK Linux and would like to understand the official camera resolution support for the AM571x, AM572x, and AM574x family.
Some TI SDK documentation and examples appear to focus on 2 MP image sensors, while I have seen references suggesting that higher-resolution sensors may also be usable.
Could you please clarify:
- Do the AM571x, AM572x, and AM574x SoCs officially support 5 MP (2592 × 1944) camera sensors?
- If yes, is this support available through the VIP/ISS/CSI-2 capture pipeline, and are there any hardware or software limitations (e.g., frame rate, interface bandwidth, ISP, or SDK support)?
- If not, is there an official TI document that specifies the maximum supported camera resolution for these SoCs?
If possible, could you also provide the relevant datasheet, TRM, or Processor SDK documentation reference?
Thank you.