Hi all,
Although searching through various posts with similar topics in the forums, I cannot get the ROV / RTA view working on the DSK6713 Platform.
If i select Tools --> ROV i get the error:
" ROV failed to start ... Unsupported ISA: 103".
I have no possibility to update to CCS V 4.1.3 , as was suggested in another Threads because according to the Wiki i can´t figure out if the DSK6713 is still supported (seems not to be the case) AND i currently have no license for a newer Version.
I use DSPBIOS Version 5.40.02.22 and CCS Studio Version 4.01.
If the ROV/RTA has never worked (or will never work) with the Versions of the tools mentioned above, or if there is a common workaround for this error, please let me know.
Regards,
Franz