Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Hi Experts:
Our customer are runing LPDDR4 stability test at their board. They found that uboot has low probability hung at their production. We has compared LPDDR4 parameter setting and insure their configure is right. below is parameter review link.
TDA4VH-Q1: uboot boot error - Processors forum - Processors - TI E2E support forums
Now i has work at EVM board reproduce customer issue. Write a script run uboot software reset at EVM board. Looks like EVM uboot run reset has same problem. Could you please help us confirm at your side and debug it together?
This is reproduce method:
- EVM board E5 version TDA4VH.
- Software 11.02.00.04 and make SD card with prebuild release. just copy boot partition and keep rootfs partion is blank.
- run below test script at minicom
minicom -D /dev/ttyUSB0 -S autoboot.scr -C ./autoboot.logautoboot.txt
change autoboot.txt to autoboot.scr - power on EVM board and capture the log.autoboot.log
we can find two kind of hung at EVM board.
TypeA: LPDDR4 init failure like below log.
SYSFW ABI: 4.0 (firmware rev 0x000b '11.2.8--v11.02.08 (Fancy Rat)')
k3_lpddr4_start: FAIL
### ERROR ### Please RESET the board ###
at this failure mode use JTAG connect MCU R5 core, we can not access 0x80000000 LPDDR4 and PC stopped at 0x41c0869c
TypeB: Hung at sysfw print log.
U-Boot SPL 2025.01-00773-gdf1fe2382304 (Dec 24 2025 - 07:50:42 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.2.8--v11.02.08 (Fancy Rat)')
At this failure mode use JTAG connect MCU R5 core, it hung at 0x41C1A024

Could you please help us analyze those uboot problem?
Best Regards!
Han Tao