Hi,
I read previous post "AM3517 NAND booting" but was not sure which step from
http://processors.wiki.ti.com/index.php/WinCE-BSP_ARM-A8_User_Guide#Flashing_the_board_through_SD_card actually does the flashing XLDRNAND.bin and EBOOTND.bin from SD to NAND. Please clarify.
2. Enable flashing by select following option from Eboot menu:
[Flash Management] -> [8]Enable flashing NK.bin
Is this "enabling flashing NK.bin" step does the flashing of all three files: NK.bin, EBOOTND.bin and XLDRNAND.bin to NAND reserved blocks?
3. Change the SDcard settings for image name to ebootnd.bin/xldrnand.bin/nk.bin from following Eboot
Menu:
[SDCard Settings] -> [Enter Filename]
I don't understand this step description. From the SD boot menu, under SDCard Settings->Show Current Settings, I have the file name is "nk.bin". Why do I have to change SDCard settings? I just want to boot from NAND. I have difficult to understand the descriptions from this step. In this step, what do I need to enter "ebootnd.bin" or "xldrnand.bin" or "nk.bin" or "ebootnd.bin/xldrnand.bin/nk.bin". Please clarify.
I made sure the NAND ECC mode is 0 (hamming 1 bit ECC) but I could not boot from NAND for some reason.
Thanks,
Dennis