I am using EDMA3 in C6455 DSP, and there is a problem of the data transferring.
Here is the phenomenon, I use EDMA3 to read data from FIFO in FPGA Virtex5 through EMIFA CE4, and the first 4 bytes are lost while the last 4 bytes repeated twice. For example, the 1K bytes data should be 0x0000 – 0x0400 (1 - 1024), but the result is 0x0004 – 0x0400 and 0x03FD – 0x0400 (1021 - 1024) repeated twice.


Here is my configuration of EMIFA:
EMIFA_CONFIGREG_STAT &= ~(0x80000000) ; //config emifa work in little endian mode
EMIFA_CONFIGREG_CE4CFG |= 0x8000030b;
The following is my configuration of EDMA3:
pEDMA3CC_PaRAM->OPT = 0x00100201; //TCINTEN=1;TCC=0;SYNCDIM=1;
pEDMA3CC_PaRAM->SRC = EMIFA_CE4_BASE_ADDR;
pEDMA3CC_PaRAM->BCNT_ACNT = 0x00010800; //ACNT=1024;BCNT=1;
pEDMA3CC_PaRAM->DST = FPGA_DATA_PING;
pEDMA3CC_PaRAM->DSTBIDX_SRCBIDX = 0x00000000;
pEDMA3CC_PaRAM->BCNTRLD_LINK = 0x00804060; //LINK=4060, PaRMA SET 3
pEDMA3CC_PaRAM->DSTCIDX_SRCCIDX = 0x0;
pEDMA3CC_PaRAM->RSVD_CCNT = 0x00000001;
The read latency of Xilinx FIFO is one clock cycle. Can anyone help to firgure out the problem?