Other Parts Discussed in Thread: TMS320C6748
Hi,
We have a Custom Built Board with TI Processor TMS320C6748 & SPI Flash memory M25P64.
We are using AISGEN to flash our program. In the Hardware we have connected ‘EN’ Pin of of Processor to ‘CS’ pin of Flash.
We made changes in ‘device_spi.c’ and re compiled the Sipwriter program. We have a new compiled SpiWriter.out file (we didn’t use Cgywin as suggested by a wiki link).
Howe ever, when we executed the ‘SpiWriter.out’ program we were able to erase and program the flash successfully. However the Boot is not happening. We used a DEBUG.gel file and got the following message.
‘ROM Status Code: 0x00000009
Description:C674X_0: GEL Output: Invalid AIS keyword’
We are not able to know where we are making the mistake. Can you help us in solving the Boot issue involving TMS320C6748 and SPI based M25P64 flash.
Regards,
Sandeep Nayak