This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I am getting this warning warning: creating output section ".bitVectors" without a SECTIONS



My linker file has following. I wish to create initialized section whose load and run addresses are different

SECTIONS
{
/* Replace the 0x0C200000 with 0x0820000 in the line below when ready to move to L2SRAM */
 GROUP (NEAR_DP): 0x0820000
 {
 .version
 .buildtime
 .neardata
 .rodata 
 .bss
 .cache_coherent_non_aggregates
 .hostShared
 }

 .csdbitreg > L2SRAM /* was MSMCSRAM2 */
 .csdtreg > L2SRAM /* was MSMCSRAM2 */

 .csdbitdebugmem > L2SRAM 
 .sect "bitVectors": load = MSMCSRAM2_NC_PHY, run = MSMCSRAM2_NC_LOG 
 
 
}