This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem in flashing PADK using CCSv4

Hi,

I am trying to flash AnaloLoopback project from Lyrtech sample projects in PADK using CCSv4 on a windows 7 machine.I did it using MakeRom.I could not find TI boot section in the .out file which is displayed in command window.Why is it so?

 After loading the Flash_AnaloLoopback.out using Load Symbols option in CCSv4,and run it,the LEDs begins to blink near to UART and MIDI. But when I make the device stand alone,it does not give me any audio output.

And I loaded the same .out file of CCSv4  in CCSv3 on  a windows Xp machine,same thing is happening.

So is this because of

(a) it is .out file from CCSv4?

(b) is it version problem of CCS?

(c) is it OS problem? I mean XP or win 7?

(d) Flash procedure of MakeRom?

Kindly help.

Thanks and Regards,

James