This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with the Real-time Video Demos

Hi,

I want to run the Real-time Video Demos using my EVM6678LE. I have prepared the software following the steps in http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.0_Demo_Guide. But I can not initial the IBL flash. When I performed the first step using the EEPROM writer utility  to write IBL image, the CCS console given me the error information that the app.dat file(at <MCSDK Video Install Dir>\demos\demoutils\IBL\evm6678l_ibl_writer which has been loaded to the memory) can not be open. 

So I have to used the newest IBL writer from MCSDK 2.0.8.20 updating the IBL and configuration. And I also set the DIP boot mode. Obviously, this did not work at all. When I verify IBL flash, the TFTP server on the PC can not get any  file request.

I think the .gel file and .dat file provided by MCSDK_VIDEO_2.0 should different with that provided by MCSDK 2.0.8.20. So do you have any idea how I should to solve this problem to make the Real-time Video Demos to run?

  • Hi li,

    Can you please try one more time by following the steps in <MCSDK Video Install Dir>\demos\demoutils\IBL_flash\evm6678l_ibl_writer\README.doc?  One note: the evmc6678l.gel file in Step 2 is located at <MCSDK Video Install Dir>\demos\demoutils\IBL_flash\evmc6678l.gel

    A few questions about your last try:

    1) Are you able to load eepromwriter_evm6678l.out successfully?

    2) You mentioned that app.dat has been loaded to the memory. Can you please provide a snapshot of the memory window starting with 0x80000000?

    3) Can you please provide the complete log when running the writer?

    Thanks,

    Hongmei

  • Hi Hongmei,

    Thank you for your reply.

    Today the most of the process is good. But after start the sendPkts.bat file, when I execute the startMplayer.bat  file to open the mediaplayer, I got the following error:

    Reference\utils\bin\startMplayers.exe customBuild\config\subj-1080p-laptop.cfg

    The system cannot execute the specified program.

    But I have checked both of this two files do exist in that path. I have no idea  how to solve this problem now.

    Just now I tried it on Windows 7, I got the similar error information:

    Reference\utils\bin\startMplayers.exe customBuild\config\subj-1080p-laptop.cfg sdp://"C:\Program Files (x86)\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\t_rtp_1_0.sdp" -geometry 352x288+200+400 -fps 30

    Caught Exception ....:The system cannot find the file specified.

    I also checked that there are lots of .sdp files include the t_rtp_1_0.sdp in "C:\Program Files (x86)\Texas Instruments\mcsdk_video_2_0_0_10\demos\demoroot\Reference\config\demo1\sdp\".

     

  • Hi li,

    This error happens if MPlayer is not installed or not installed at C:\Program Files\MPlayer for Windows. Please follow "http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.0_Demo_Guide#Preparing_the_PC" to download and install MPlayer. Make sure "C:\Program Files\MPlayer for Windows\mplayer\mplayer.exe" exists after the installation.

    Thanks,

    Hongmei

  • Thank you for your response Hongmei,

    But I did install the MPlayer at C:\Program Files\MPlayer for Windows. Now I even can use the mplayer.exe to open the following 4 streams manually in command line.

    \demoroot\Reference\config\demo1\sdp\t_rtp_0_0_xp.sdp,

    \demoroot\Reference\config\demo1\sdp\t_rtp_0_1_xp.sdp,

    \demoroot\Reference\config\demo1\sdp\t_rtp_0_2_xp.sdp,

    \demoroot\Reference\config\demo1\sdp\t_rtp_0_3_xp.sdp,

    However, I can not open the other 12 streams using mplayer.exe manually.  I tried several times, it still did not work.

    After that, I compared the four files above with the other 12 .sdp files. I found the other 12 files will open the rtp streams at the IP address 192.168.0.120~192.168.0.124 while the above four stream files use the IP address 192.168.0.102 which is a local IP address. Is it correct? When I use mplayer.exe open the rtp stream for rtp_1_0.sdp file, using the command:mplayer.exe rtp://192.168.0.120:32770, I get the information"Timeout! No data from host 192.168.0.120 rtp_streaming_start failed, No stream found to handle url rtp://192.168.0.120:32770".

     So I have 3 questions:

    1.  I can not  using start Mplayers.exe to open the mplayer as I installed MPlayer at the right path. Do you have any debug solution for me to figure out what the problem is?

    2. How can I open the other 12 streams through other methods? Because now I can not sure if the other 12 streams were sent from my EVM board.

    3. If the ip address in the .sdp files are correct?

    Thank you in advance.

  • I just now have reinstalled all the software and the XP system. The results is same when I input startMplayers.bat in command line:"The system cannot execute the specified program".

    I am totally no idea, please help me, Hongmei!

  • Hi Hongmei,

    I just now found the reason why the startMplayers.bat can not be executed. That is because my system has no dotnetframework and I need to reinstall vcredist_x86.exe.

    However, I still only have 4 streams and that is the same problem with this thread http://www.deyisupport.com/question_answer/f/53/t/7344.aspx. There are 12 streams missed. 

    Can you help me how to find them out?

  • Hi li,

    Good to know that you have fixed the issue with running MPlayer. For the missing streams, can you please first refer to the following link? http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/189161.aspx. 

    If it's still not working, please provide the logs as specified in the above post.

    Thanks,

    Hongmei

  • Hi li,

    Just want to follow up to see if you have brought up the real-time video demo. Please let us know if any help is needed.

    Thanks,

    Hongmei