This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

onvif discovery issue of DM36X IPNC V3.0



hi all:

   I use IPNC V3.0 REF, now open the ONVIF TEST TOOLS 1.02, if I press "Discover Devices", it can get nothing.  it can not discover my IPC,  my IPC uses static IP(192.168.1.168),  but if I fill "192.168.1.168" in  "Device IP", and press "Probe",  then can get response from my IPC, and display regarding infomations on the "Discovery" page, such as "IP, UUID", BRAND, and so on. 

  Also, I use other NVR which supports onvif 2.0 to discover my IPC, can not discovery my IPC.  My IPC can not respond to the "239.255.255.250 : 3702" multicast info send by NVR or ONVIF TEST TOOLS 1.02  on the local network,

 who can give me some suggestions please ?  Thanks

REGARDS

Steven