Hi,
We want to use the All ADC Channels in "4-wire TSC with 4 general-purpose ADC channels" mode.
Because, we have the 4-Wite Touch SCreen (Interfaced to AIN0, AIN1, AIN2 and AIN3) and 4 no's of Temprature Sensors (NTC Resistors) (Interfaced to AIN4, AIN5, AIN6 and AIN7).
Is the Linux BSP Supports TSC and ADC are working same time?.
If not, Now, How i can program the Linux BSP Drivers to support 4-Wire TSC and another 4-ADC working simultaneusly?.
Is there any standlaone example for using the TSC and ADC's, to start Linux BSP Driver Modification?.
Thanks
Reddy