Hi
Whats the advantage of moving from twl6030 to twl6032 PMIC
Is there a driver patch [twl-core.c] supporting twl6032 PMIC for Linux kernel Versions?
Regards,
Kavitha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kavitha,
The twl6032 is used with OMAP4470 because the 4470 requires more current to drive its MPU during corner cases and twl6032 can do this. 6030 may not be enough at times. If you are using 4460 or 4430, the twl6032 is not needed for OMAP.
The current releases for the kernel already include the code dealing with twl6032.
JB kernel base directory: http://git.omapzoom.org/?p=kernel/omap.git;a=tree;h=refs/heads/p-android-omap-3.4;hb=p-android-omap-3.4
ICS kernel base directory: http://git.omapzoom.org/?p=kernel/omap.git;a=tree;h=refs/heads/p-android-omap-3.0;hb=refs/heads/p-android-omap-3.0
Here's the setup for the OMAP development processor boards: