Other Parts Discussed in Thread: TVP7002, TLC59108
Hi,
I am using gstreamer to capture and preview live 720p60 video on the DM8148 EVM (I have the HDVICP2 running at 410 MHz), and am routinely running into a loss of buffers issue (see attached text). The preview mode starts to work (I get a couple of frames of video on the LCD) before the error. Is there something I need to add to the stream request for buffering or using the VPSS?
-Mike
---- Output
root@dm814x-evm:~# gst-launch v4l2src device="/dev/video0" always-copy=false queue-size=16 num-buffers=5000 ! 'video/x-raw-yuv-strided,format=(fourcc)NV12,width=1280,height=720,framerate=(fraction)60/1' ! omxbufferalloc numBuffers=16 ! omx_scaler ! video/x-raw-yuv,width=800,height=480 ! omx_ctrl display-mode=OMX_DC_MODE_720P_60 display-device=LCD ! gstperf ! omx_videosink sync=false display-device=LCD
Setting pipeline to PAUSED ...
tvp7002_s_dv_preset: 8 Mode set is 720P60
allocating 16 buffers of size:1382400!!
allocated outbuf:0x441b8080
allocated outbuf:0x44309880
allocated outbuf:0x4445b080
allocated outbuf:0x445ac880
allocated outbuf:0x------------[ cut here ]------------
WARNING: at kernel/softirq.c:159 local_bh_enable+0x54/0xc4()
Modules linked in: bufferclass_ti omaplfb pvrsrvkm tlc59108 ti81xxhdmi ti81xxvin ti81xxvo ti81xxfb vpss tvp7002 syslink ipv6
Backtrace:
[<c004abd0>] (dump_backtrace+0x0/0x110) from [<c03d8ee8>] (dump_stack+0x18/0x1c)
r7:00000000 r6:c0074d08 r5:c04ae5e8 r4:0000009f
[<c03d8ed0>] (dump_stack+0x0/0x1c) from [<c006f770>] (warn_slowpath_common+0x54/0x6c)
[<c006f71c>] (warn_slowpath_common+0x0/0x6c) from [<c006f7ac>] (warn_slowpath_null+0x24/0x2c)
r9:c056726c r8:d088c780 r7:0000000d r6:ccaa2900 r5:c053e8a0
r4:c0592a00
[<c006f788>] (warn_slowpath_null+0x0/0x2c) from [<c0074d08>] (local_bh_enable+0x54/0xc4)
[<c0074cb4>] (local_bh_enable+0x0/0xc4) from [<c00695e8>] (omap_mbox_msg_send+0xcc/0xdc)
r5:c053e8a0 r4:00000000
[<c006951c>] (omap_mbox_msg_send+0x0/0xdc) from [<c030ba0c>] (notify_shm_drv_send_event+0x1c8/0x208)
r5:00000001 r4:00000000
[<c030b844>] (notify_shm_drv_send_event+0x0/0x208) from [<c030919c>] (notify_send_event+0x114/0x26c)
[<c0309088>] (notify_send_event+0x0/0x26c) from [<bf196a08>] (vps_fvid2_queue+0xe4/0x21c [vpss])
[<bf196924>] (vps_fvid2_queue+0x0/0x21c [vpss]) from [<bf19fccc>] (capture_queue+0x50/0x64 [vpss])
r8:bf1d1524 r7:60000013 r6:cc2ce580 r5:00000000 r4:cb780400
[<bf19fc7c>] (capture_queue+0x0/0x64 [vpss]) from [<bf1d02d0>] (ti81xxvin_buffer_queue+0x9c/0xe8 [ti81xxvin])
r5:cb75b800 r4:cb780400
[<bf1d0234>] (ti81xxvin_buffer_queue+0x0/0xe8 [ti81xxvin]) from [<c02e2994>] (videobuf_streamon+0x80/0xd0)
r7:60000013 r6:cb75b9c4 r5:cb75b904 r4:cc2ce580
[<c02e2914>] (videobuf_streamon+0x0/0xd0) from [<bf1cfd48>] (vidioc_streamon+0x244/0x400 [ti81xxvin])
r7:cc0d6200 r6:00000001 r5:cb75b800 r4:cb75b904
[<bf1cfb04>] (vidioc_streamon+0x0/0x400 [ti81xxvin]) from [<c02d8224>] (__video_do_ioctl+0x164c/0x3fe0)
r6:40045612 r5:00000000 r4:00000001
[<c02d6bd8>] (__video_do_ioctl+0x0/0x3fe0) from [<c02d69c8>] (__video_usercopy+0x2e4/0x428)
[<c02d66e4>] (__video_usercopy+0x0/0x428) from [<c02d6b3c>] (video_ioctl2+0x30/0x38)
[<c02d6b0c>] (video_ioctl2+0x0/0x38) from [<c02d5b7c>] (v4l2_ioctl+0xe8/0x11c)
r5:cc0d6200 r4:cc0c5200
[<c02d5a94>] (v4l2_ioctl+0x0/0x11c) from [<c00d6724>] (vfs_ioctl+0x28/0x44)
r9:c7156000 r8:0001cc70 r7:0000001b r6:0000001b r5:cc0c5200
r4:00000000
[<c00d66fc>] (vfs_ioctl+0x0/0x44) from [<c00d6e34>] (do_vfs_ioctl+0x500/0x540)
[<c00d6934>] (do_vfs_ioctl+0x0/0x540) from [<c00d6ecc>] (sys_ioctl+0x58/0x7c)
[<c00d6e74>] (sys_ioctl+0x0/0x7c) from [<c0046e00>] (ret_fast_syscall+0x0/0x30)
r8:c0046fa8 r7:00000036 r6:0001cc58 r5:00020500 r4:00126b48
---[ end trace 454b631a921228db ]---
446fe080
allocated outbuf:0x4484f880
allocated outbuf:0x449a1080
allocated outbuf:0x44af2880
allocated outbuf:0x44c44080
allocated outbuf:0x44d95880
allocated outbuf:0x44ee7080
allocated outbuf:0x45038880
allocated outbuf:0x4518a080
allocated outbuf:0x452db880
allocated outbuf:0x4542d080
allocated outbuf:0x4557e880
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
kernel BUG at drivers/media/video/ti81xx/ti81xxvin_main.c:842!
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = c7114000
[00000000] *pgd=8787f031, *pte=00000000, *ppte=00000000
Internal error: Oops: 817 [#1]
last sysfs file: /sys/module/pvrsrvkm/initstate
Modules linked in: bufferclass_ti omaplfb pvrsrvkm tlc59108 ti81xxhdmi ti81xxvin ti81xxvo ti81xxfb vpss tvp7002 syslink ipv6
CPU: 0 Tainted: G W (2.6.37+ #42)
PC is at __bug+0x20/0x2c
LR is at release_console_sem+0x198/0x1ac
pc : [<c004a94c>] lr : [<c007008c>] psr: 20000013
sp : c701fb90 ip : c701fac8 fp : c701fb9c
r10: 00000000 r9 : c701fe08 r8 : c701fe08
r7 : cb75b904 r6 : cc15f600 r5 : cb75b800 r4 : cb780400
r3 : 00000000 r2 : 00000001 r1 : 00008e00 r0 : 00000045
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 87114019 DAC: 00000015
Process gst-launch-0.10 (pid: 1487, stack limit = 0xc701e2e8)
Stack: (0xc701fb90 to 0xc7020000)
fb80: c701fbbc c701fba0 bf1d02e4 c004a938
fba0: cc15f600 20000013 00000000 cb75b904 c701fbe4 c701fbc0 c02e32ac bf1d0240
fbc0: 00000001 cb75b800 c7018540 c701fe08 bf1d1524 c701fe08 c701fc4c c701fbe8
fbe0: bf1d002c c02e2f3c 43737000 00000004 00000001 00000000 00000000 00000000
fc00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000002
fc20: 446fe080 00000000 00000000 00000000 bf1cff94 c044560f c044560f cc0d6200
fc40: c701fdf4 c701fc50 c02d7f60 bf1cffa0 53555f54 54524f48 50004e34 52535256
fc60: 52455f56 5f524f52 41564e49 5f44494c 49564544 44494543 33697500 76654432
fc80: 49656369 56500044 56525352 4655425f 43524546 5353414c 5245505f 544e4f43
fca0: 5f545845 4f464e49 4741545f 52565000 c7036080 00000101 00000000 00000101
fcc0: 00000024 00000001 c701fce4 c701fcd8 c0540cd0 c70402fc 5dd00028 00000001
fce0: c70402f8 00000000 c701fd1c c701fcf8 c006bec8 c01d70f4 c7040304 c7040000
fd00: c0540c88 00000001 c7040030 0017d438 cca77340 c7040030 cca77370 c0540c88
fd20: cca77340 c7040030 c701fd5c c701fd38 c006ba10 c0069e1c c0540c88 c03e1968
fd40: cca77340 cca77340 00000000 00000000 fffffffd 00000000 c701fd8c c701fd68
fd60: c03dd00c c00421c4 c704601c cca77340 00000015 c044560f cc0c5200 c7018540
fd80: c701fda4 c701fd90 c03dd06c c03dcfe4 00000000 c701fda0 c701fdbc c701fda8
fda0: c03dd094 c03dd05c ccbcd000 cca77340 c701fde4 c701fdc0 c03d97a4 c006d260
fdc0: c701e000 7fffffff d5e4a010 00000044 00000000 c044560f 00000000 00000000
fde0: 00000000 c701fe08 c701feb4 c701fdf8 c02d69c8 c02d6be4 c02d6bd8 0017e998
fe00: cc0c5200 00000003 00000004 00000001 00000000 00000000 00000000 00000000
fe20: 00000000 00000000 00000000 00000000 00000000 00000000 00000002 446fe080
fe40: 00000000 00000000 00000000 c701fe58 bf0745c8 bf0729b4 bf074668 bf072900
fe60: c701fea4 d0b2f000 00000000 d5c05700 c701fea4 c701fe80 bf081748 bf072900
fe80: 00000000 c018f361 412d4d60 cc0c5200 0017e998 bf1d2408 c044560f 0017e998
fea0: c701e000 00000000 c701fecc c701feb8 c02d6b3c c02d66f0 cc0c5200 cc0d6200
fec0: c701fef4 c701fed0 c02d5b7c c02d6b18 00000000 cc0c5200 0000001c 0000001c
fee0: 0017e998 c701e000 c701ff04 c701fef8 c00d6724 c02d5aa0 c701ff74 c701ff08
ff00: c00d6e34 c00d6708 0b460d1c 00000067 0b460d1c 00000067 0b460d1c 00000067
ff20: 0000034c c052c9a0 00000000 00000000 00000043 003d0f00 c701e000 00000000
ff40: c701ff5c c701ff50 00000001 00000000 0017e998 c044560f 0000001c cc0c5200
ff60: c701e000 00000000 c701ffa4 c701ff78 c00d6ecc c00d6940 c701ff94 00000001
ff80: c00749d8 00000004 0000034c 405f08d4 00000036 c0046fa8 00000000 c701ffa8
ffa0: c0046e00 c00d6e80 00000004 0000034c 0000001c c044560f 0017e998 446fe080
ffc0: 00000004 0000034c 405f08d4 00000036 00126b48 beeb6d70 0000034c 412d4c2c
ffe0: 0017e940 412d4a70 405d52e8 4052daec 60000010 0000001c 5f535041 45474150
Backtrace:
[<c004a92c>] (__bug+0x0/0x2c) from [<bf1d02e4>] (ti81xxvin_buffer_queue+0xb0/0xe8 [ti81xxvin])
[<bf1d0234>] (ti81xxvin_buffer_queue+0x0/0xe8 [ti81xxvin]) from [<c02e32ac>] (videobuf_qbuf+0x37c/0x43c)
r7:cb75b904 r6:00000000 r5:20000013 r4:cc15f600
[<c02e2f30>] (videobuf_qbuf+0x0/0x43c) from [<bf1d002c>] (vidioc_qbuf+0x98/0xb4 [ti81xxvin])
r9:c701fe08 r8:bf1d1524 r7:c701fe08 r6:c7018540 r5:cb75b800
r4:00000001
[<bf1cff94>] (vidioc_qbuf+0x0/0xb4 [ti81xxvin]) from [<c02d7f60>] (__video_do_ioctl+0x1388/0x3fe0)
r7:cc0d6200 r6:c044560f r5:c044560f r4:bf1cff94
[<c02d6bd8>] (__video_do_ioctl+0x0/0x3fe0) from [<c02d69c8>] (__video_usercopy+0x2e4/0x428)
[<c02d66e4>] (__video_usercopy+0x0/0x428) from [<c02d6b3c>] (video_ioctl2+0x30/0x38)
[<c02d6b0c>] (video_ioctl2+0x0/0x38) from [<c02d5b7c>] (v4l2_ioctl+0xe8/0x11c)
r5:cc0d6200 r4:cc0c5200
[<c02d5a94>] (v4l2_ioctl+0x0/0x11c) from [<c00d6724>] (vfs_ioctl+0x28/0x44)
r9:c701e000 r8:0017e998 r7:0000001c r6:0000001c r5:cc0c5200
r4:00000000
[<c00d66fc>] (vfs_ioctl+0x0/0x44) from [<c00d6e34>] (do_vfs_ioctl+0x500/0x540)
[<c00d6934>] (do_vfs_ioctl+0x0/0x540) from [<c00d6ecc>] (sys_ioctl+0x58/0x7c)
[<c00d6e74>] (sys_ioctl+0x0/0x7c) from [<c0046e00>] (ret_fast_syscall+0x0/0x30)
r8:c0046fa8 r7:00000036 r6:405f08d4 r5:0000034c r4:00000004
Code: e1a01000 e59f000c eb0e39c7 e3a03000 (e5833000)
---[ end trace 454b631a921228dc ]---
ti81xxvin: list empty