Other Parts Discussed in Thread: 4430, 4460
Hi,
I have managed to boot 4AJ.1.1 on Blaze from eMMC but I have no success in booting it up on SD card.
I tried two different ways using SD card.
1. Manually partition SD card according to release note guild line.
2. Use fastboot to load images into SD card.
Here is the result;
Method 1:
Blaze managed to the Android file system after some modification on omap4430sdp.h and mmc.c.
FULL message can be found in the attachment.
Method 2;
Blaze managed to partition onto my SD card. After reboot, It is still able to detect and display the partition table on the SD card but for unknown reason it still load the Android file system on eMMC.
***I have ensure the S2 switch is set correctly when booting the Blaze from the SD card.
So can anyone give me some tips how to overcome those problem I am facing.
Best Regards
Yong