This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ETHERNET BOOT RBL AND IBL



Dear sirs,
I have two problems on the evaluation board and I want to ask you some feedback.

1) The RBL in ethernet boot mode. Did you have tested it? Can you give me feedback on this please?
I did the procedure written in the mcsdk_2_01_01_04 but the DSP don't boot,. The procedure in follow describe the steps:

ROM Ethernet boot example "ti\mcsdk_2_01_01_04\tools\boot_loader\examples\ethernet\docs"

A simple example demonstrating ROM Ethernet boot.
Directory structure:

docs - directory contains the README.txt
simple - directory contains the batch/make file to build the simple example
Utilities - directory contains the utilities to convert the hex6x boot table file
to the Ethernet boot format data file:

bconvert64x.exe - Convert a hex6x boot table file into the format required
by the c6x chip boot loader.
bootpacket.exe - Convert a boot table to Ethernet boot format

Steps to build the example:

1. Run "simple.bat" under "tools\boot_loader\examples\ethernet\simple\". This will build the simple.out and use
hex6x.exe (delivered in CG tools package) to convert the .out to a boot table file, and then use the
bconvert64x.exe/bootpacket.exe to convert the hex6x boot table file to the Ethernet boot format data file,
simple.eth.

Steps to send the simple.eth from the Host to the target DSP

1. Boot the target DSP in ROM Ethernet boot mode.

The DIP switch setting for C6657 EVM is:
SW3(pin1, pin2, pin3, pin4, pin5, pin6, pin7, pin8): off, on, off, on, on, on, on, off
SW5(pin1, pin2, pin3, pin4, pin5, pin6, pin7, pin8): on, off, on, off, off, on, on, on

2. Once the DSP boots up, it transmits BOOTP packet at regular interval which will have the MAC ID of the DSP.

3. Add an ARP entry for the DSP MAC address associating with an IP local to the host. For example if the host PC's
IP is 192.168.1.1, then add an ARP entry with the DSP's MAC address associated with IP address 192.168.1.2.

4. Use the pcsendpkt.exe to send the image to the DSP using the associated IP address. For example
pcsendpkt.exe simple.eth 192.168.1.2 (After this the DSP continue to send Bootp Packet)

5. Use CCS to connect the EVM, and check that A1 register is set to 0x11223344, that confirms the simple program
is received and booted by the ROM boot loader.(The value in A1 reg is not 0x11223344)

Notes:
1. In order to compile the pcsendpkt.c file please compile with -lwsock32 option for using windows socket. (I tried to recomipile it but I don't note any changes, olso I tried to change the src and dest port but nothing changes)
2. Please refer to the C66x DSP Bootloader User's Guide (http://www.ti.com/litv/pdf/sprugy5) for more details.(I red itfirst)
3. Please refer to C6678L/C6670L/C6657L EVM boot mode dip switch settings:
http://processors.wiki.ti.com/index.php/TMDSEVM6657L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings

and User's Guide for more details:
http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide

2) The second problem is, always arrowed to the boot but on IBL etherneth Boot.
I did the procedure written at page 81 and page 113 of BIOS MCSDK 2.0 User GUIDE
I have the same problem and the same questions : The DSP don't boot, can you give feedback on it?