This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can dm8168 be able to run Codec Engine program with video capture and display using EZSDK 5.04 ?

Dear all

I use EZSDK 5.04 ,  in my program ,I could capture and display video.  On A8 side , now I can get the video frame  through HDVPSS .   But I also want to run video algorithm  on C674x DSP side ,so I want to use Codec Engine  framework.

Then I have found a document named DM816x EZ Software Developers Guide ,it presents "

Note! The Codec Engine examples cannot be run out with graphics. Please execute the following steps to

teardown the graphics plane and ensure that no firmware is running.

target # /etc/init.d/pvr-init stop

target # /etc/init.d/matrix-gui-e stop

target # /etc/init.d/load-hd-firmware.sh stop"  ,

graphics have been shut down ,  I can't capture  video ,  if I don't shut down graphics ,my CE engine even couldn't open . I want to run codec engine to run algorithm on DSP side  , and at same time do  videocapture on A8 side througth HDVPSS  , then  output the video output  using FB.  It seems like a conflict between video capture and program based on CE .   how can the process be realized.

 
                                                                                                                    yours sincerely,saisai liang