This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does Scalar Component support multiple input/output ports?



Hi,

 I have a question about the scalar component. In the OMX_05_02_00_38_UserGuide, it is said that both this component could have up to 16 inports and outports. I try to set the inport/outport number to 4 and set params of each port. There is no error but the result shows only the first port works.

  So, can anyone tell me if the scalar component supports multiple ports?

  Appreciate for your reply!