Hello,
I need to check if my camera works properly. I'm looking for a code where I may capture data from my camera (vpif) and send it to VGA to display on my monitor. Can somebody guide me? Thank you. My email: osjan1@o2.pl
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to check if my camera works properly. I'm looking for a code where I may capture data from my camera (vpif) and send it to VGA to display on my monitor. Can somebody guide me? Thank you. My email: osjan1@o2.pl
Hi Mark,
You may find these links useful.
http://e2e.ti.com/support/embedded/linux/f/354/t/40151.aspx
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/180709.aspx
Regards,
Shankari.
---------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
---------------------------------------------------------------------------------
Hello,
Thank you for reply, but I need example how to implement OV5640 (implementation code). I can't even find proper user guide for this.
Regards,
Okay, I try to implement code for camera, in this code I want to read the camera ID:
in main():
I2CPinMuxSetup(0);
I2COV5640IfInit(SOC_I2C_0_REGS, INT_CHANNEL_I2C,0x5640);
ov5640_detect(SOC_I2C_0_REGS);//is camera?
static int ov5640_detect(unsigned int baseAddr)
{
unsigned short val = 0;
val = (OV5640RegRead(baseAddr, REG_CHIP_ID_MSB) << 8) + OV5640RegRead(baseAddr, REG_CHIP_ID_LSB);
if (OV5640_CHIP_ID != val) {return 1;}
return 0;
}
unsigned char OV5640RegRead(unsigned int baseAddr, unsigned int regAddr)
{
/* Send the register address */
slaveDatas[0] = regAddr;
I2COV5640SendBlocking(baseAddr, 1);
/* Receive the register contents in slaveData */
I2COV5640RcvBlocking(baseAddr, 1);
return (slaveDatas[0]);
}
void I2COV5640Isr(void)
{
unsigned int intCode = 0;
unsigned int sysIntNum = 0;
intCode = 0;
/* Get interrupt vector code */
intCode = I2CInterruptVectorGet(SOC_I2C_0_REGS);
sysIntNum = SYS_INT_I2C0_INT;
while(intCode!=0)
{
IntEventClear(sysIntNum);
if (intCode == I2C_INTCODE_TX_READY)
{
I2CMasterDataPut(SOC_I2C_0_REGS, 0x300A);
dataIdxx++;
}
if(intCode == 4)
{
slaveDatas[1] = I2CMasterDataGet(SOC_I2C_0_REGS);
dataIdxx++;
}
if (intCode == 6)
{
I2CMasterIntDisableEx(SOC_I2C_0_REGS, I2C_INT_TRANSMIT_READY
| I2C_INT_DATA_READY);
txCompFlagg = 0;
}
intCode = I2CInterruptVectorGet(SOC_I2C_0_REGS);
}
}
Functions are from codecif.c. When I sent I2CMasterDataPut(SOC_I2C_0_REGS, 0x300A) in interrupt I got NACK (code 2) and later code 3 and I can't get any data. What I'm doing wrong? Is this problem with the code or with hardware? Thank you.
Hi Mark,
From this post and your question in this other one (http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/180709.aspx) I think that both of us are facing the same problem.
I'm trying to capture raw data from a OV7692 sensor and you can see here (http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/257714/924817.aspx#924817) that I'm also not able to get any VPIF interrupt.
While we pray for an answer from TI's support, please check if you might also have the issue with the vertical blanking time in your sensor. I'll keep you informed of any progress on my side and I will be very grateful if you could also inform me on your progress.
Regards,
Erik
void I2C_MT9M024_Init(unsigned int baseAddr, unsigned int intCh,
unsigned int slaveAddr)
{
unsigned int sysIntNum = 0;
/* Put i2c in reset/disabled state */
I2CMasterDisable(baseAddr);
/* Configure i2c bus speed to 100Khz */
I2CMasterInitExpClk(baseAddr, 24000000, 8000000, 100000);
/* Set i2c slave address */
I2CMasterSlaveAddrSet(baseAddr, slaveAddr);
I2CMasterEnable(baseAddr);
/*
** Setup the interrupt in AINTC for the i2c module.
** If another instance is to be added, this shall include
** checking for the other instance base address also.
*/
if(SOC_I2C_0_REGS == baseAddr)
{
#ifdef _TMS320C6X
sysIntNum = SYS_INT_I2C0_INT;
#else
sysIntNum = SYS_INT_I2CINT0;
#endif
}
I2CCodecIntSetup(sysIntNum, intCh);
UARTPuts("i2c for mt9 done\n ", -1);
}
MT9M024_Init Function
void MT9M024_Init(unsigned int baseAddr)
{
CameraRegWrite(baseAddr,0x301A, 0x0059);
Delay(1000000);
CameraRegWrite(baseAddr,0x301A, 0x0058);
}
CameraRegWrite Function
void CameraRegWrite (unsigned int baseAddr, unsigned int regAddr, unsigned int regData)
{
#ifdef CODEC_INTERFACE_I2C
/* Send the register address and data
* MSB is transmitted first */
//16-bit register address
slaveData[0] = ((regAddr & 0xFF00 ) >> 8); //msb
slaveData[1] = (regAddr & 0x00FF); //lsb
//16-bot data
slaveData[2] = ((regData & 0xFF00 ) >> 8); //msb
slaveData[3] = (regData & 0x00FF); //lsb
I2CCodecSendBlocking(baseAddr, 4);
#endif
}
It seems as if the receiver cannot recieve anything....I would appreciate any suggestions for what I am doing wrong.
Hello,
just an update...The i2c code was fine, the problem was that I was using a non-valid slave address for the sensor.
Hello Katerina,
we also try to run LI Dual from leopard imagin but we did not success. Do you have working driver for another device? It works only with Leopard modules :-/ We wanted to connect it do a BB-xM and now we are trying to connect it to iMX6. Is it possible to discuss it via email? koutnym [ at ] feec.vutbr.cz
We would like to use it for dept map computation.
thank you, Martin
Hello Martin,
I think it would be better to discuss it here in case someone else is interested too.
My progress so far with the LI-MT9M024DUAL is i2c communication ,but no streaming....
The i2c code from Staterware works fine ,the thing is that instead of 0x20u you have to use 0x90u as a slave address for the device.
I would recommend you to have a look in the following post for information about getting frames from your camera header.
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/251424/993960.aspx#993960
In addition ,in this thread I have posted a github link for a driver released from Aptina for BB-xM .The driver is for MT9M034 which has the same registers as the two MT9M024 that are interfaced in LI-MT9M024DUAL.
Kind Regards,
Katerina Trilyraki
Hello Katerina,
I am sorry for delay. I think, the adress is not problem. In origin driver from Leopard, the address is defined by board you used with:
#ifdef BOARD_AP_IPNC
#define IMGS_I2C_ADDR (0x20)//(0x90)
#endif
#ifdef BOARD_TI_EVM
#define IMGS_I2C_ADDR (0xBA)
#endif
The original driver from Leopard
We try to transform the driver for V4L becouse we want to used BB-XM and then iMX6 for communication with the dual camera board.
At this time, we are able to communicate but we are not able to get video data. We think, there could be problem with 1V8 vs 3V3 data links.
I am sorry for code from us, it is not good written becouse we are still in developing phase. Hope the source codes helps to run Dual sensor ;-)
Hello Martin,
I was working with LI-M024DUAL and OMAPL138-LCDK and I was able to communicate with the sensor via I2C with the address 0x90 instead of 0x20....
I am sure that the communication was established because I have read the chip version from the sensor and also every register whose value I have altered.
I remember to have seen in a datasheet (which I can't locate now) from Aptina that the I2C slave address of a sensor is depending on whether the sensor's Saddr pin is pulled low or high.
The LI-M024DUAL module has Saddr pin driven low,which I think it mean that the sensor's slave address is 0x90 instead of 0x20.
Could you please investigated further the I2C part of the communication and inform me about the results.
Kind Regards,
Katerina