We are developing a custom AM335x board (based on the BeagleBone and AM335x Start Kit) with a Micron MT29F2G08ABAEAWP 2Gbit NAND chip.
This is an 8 bit device, connected to CS0, as follows:-
I have compiled the latest git U-Boot 2013.01, and (with a custom config, board.c and mux.c file - attached below) I am able to boot from MMC (SYSBOOT[4:0] = 10111) :-
U-Boot SPL 2013.01-00291-g9609fad-dirty (Feb 15 2013 - 12:30:45)
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01-00291-g9609fad-dirty (Feb 15 2013 - 12:30:45)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401000 using PIO, IRQ 0
Net: cpsw, usb_ether
U-Boot#
I can also write the same MLO and u-boot.img to our NAND device:-
U-Boot#nand info
Device 0: nand0, sector size 128 KiB
Page size 2048 b
OOB size 64 b
Erase size 131072 b
U-Boot# fatload mmc 0 82000000 MLO
reading MLO
75724 bytes read in 14 ms (5.2 MiB/s)
U-Boot# nandecc hw 2
HW BCH8 selected
U-Boot# nand erase 0 200000
NAND erase: device 0 offset 0x0, size 0x200000
Erasing at 0x1e0000 -- 100% complete.
OK
U-Boot# nand write 82000000 0 20000
NAND write: device 0 offset 0x0, size 0x20000
131072 bytes written: OK
U-Boot# nand dump 0
Page 00000000 dump:
40 00 00 00 0c 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 43 48 53 45 54 54 49 4e 47 53 00 00
ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
c1 c0 c0 c0 00 01 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
....
But when I switch our board to NAND booting (SYSBOOT[4:0] = 10011), I get nothing on UART0.
Using a scope, I can see that the NAND signals are being toggled (in a burst of activity every 10ms).
The Micron NAND device does have it's own internal ECC hardware, but I think it is OFF by default.
I have tried SYSBOOT[9] at both a '0' and a '1' (to turn ECC mode on / off) but neither mode works.
Can anyone assist me in tracking down what might be wrong ?
Cheers
Mark JACKSON
/* * board.c * * Board functions for Newflow NanoBone board * * Copyright (C) 2013, Newflow Ltd - http://www.newflow.co.uk/ * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR /PURPOSE. See the * GNU General Public License for more details. */ #include <common.h> #include <errno.h> #include <asm/arch/clock.h> #include <asm/arch/cpu.h> #include <asm/arch/ddr_defs.h> #include <asm/arch/gpio.h> #include <asm/arch/hardware.h> #include <asm/arch/sys_proto.h> #include <asm/arch/mem.h> #include <asm/arch/mmc_host_def.h> #include <asm/arch/omap.h> #include <asm/emif.h> #include <asm/gpio.h> #include <asm/io.h> #include <cpsw.h> #include <i2c.h> #include <miiphy.h> #include <spl.h> #include "board.h" DECLARE_GLOBAL_DATA_PTR; /* NAND config */ #define NAND_CS 0 #define NAND_BASE 0x00000000 #define NAND_SIZE GPMC_SIZE_256M static u32 gpmc_nand_config[GPMC_MAX_REG] = { 0x00000800, 0x001e1e00, 0x001e1e00, 0x16051807, 0x00151e1e, 0x16000f80, 0 }; /* FRAM config */ #define FRAM_CS 1 #define FRAM_BASE 0x10000000 #define FRAM_SIZE GPMC_SIZE_16M static u32 gpmc_fram_config[GPMC_MAX_REG] = { 0x00001200, 0x00101000, 0x00020201, 0x0f030f03, 0x010d1010, 0x000301c0, 0 }; /* NOR Flash config */ #define NOR_CS 3 #define NOR_BASE 0x14000000 #define NOR_SIZE GPMC_SIZE_64M static u32 gpmc_nor_config[GPMC_MAX_REG] = { 0x00001200, 0x00101004, 0x00020201, 0x10041004, 0x010f1010, 0x000601c0, 0 }; static struct wd_timer *wdtimer = (struct wd_timer *)WDT_BASE; #ifdef CONFIG_SPL_BUILD static struct uart_sys *uart_base = (struct uart_sys *)DEFAULT_UART_BASE; #endif /* MII mode defines */ #define PORT1_MII_MODE_ENABLE 0x0 #define PORT2_MII_MODE_ENABLE 0x0 #define PORT1_RMII_MODE_ENABLE 0x1 #define PORT2_RMII_MODE_ENABLE 0x4 #define PORT1_RGMII_MODE_ENABLE 0x12 #define PORT2_RGMII_MODE_ENABLE 0x28 static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE; /* UART Defines */ #ifdef CONFIG_SPL_BUILD #define UART_RESET (0x1 << 1) #define UART_CLK_RUNNING_MASK 0x1 #define UART_SMART_IDLE_EN (0x1 << 0x3) static void rtc32k_enable(void) { struct rtc_regs *rtc = (struct rtc_regs *)AM335X_RTC_BASE; /* * Unlock the RTC's registers. For more details please see the * RTC_SS section of the TRM. In order to unlock we need to * write these specific values (keys) in this order. */ writel(0x83e70b13, &rtc->kick0r); writel(0x95a4f1e0, &rtc->kick1r); /* Enable the RTC 32K OSC by setting bits 3 and 6. */ writel((1 << 3) | (1 << 6), &rtc->osc); } static const struct ddr_data ddr3_data = { .datardsratio0 = MT41J128MJT125_RD_DQS, .datawdsratio0 = MT41J128MJT125_WR_DQS, .datafwsratio0 = MT41J128MJT125_PHY_FIFO_WE, .datawrsratio0 = MT41J128MJT125_PHY_WR_DATA, .datadldiff0 = PHY_DLL_LOCK_DIFF, }; static const struct cmd_control ddr3_cmd_ctrl_data = { .cmd0csratio = MT41J128MJT125_RATIO, .cmd0dldiff = MT41J128MJT125_DLL_LOCK_DIFF, .cmd0iclkout = MT41J128MJT125_INVERT_CLKOUT, .cmd1csratio = MT41J128MJT125_RATIO, .cmd1dldiff = MT41J128MJT125_DLL_LOCK_DIFF, .cmd1iclkout = MT41J128MJT125_INVERT_CLKOUT, .cmd2csratio = MT41J128MJT125_RATIO, .cmd2dldiff = MT41J128MJT125_DLL_LOCK_DIFF, .cmd2iclkout = MT41J128MJT125_INVERT_CLKOUT, }; static struct emif_regs ddr3_emif_reg_data = { .sdram_config = MT41J128MJT125_EMIF_SDCFG, .ref_ctrl = MT41J128MJT125_EMIF_SDREF, .sdram_tim1 = MT41J128MJT125_EMIF_TIM1, .sdram_tim2 = MT41J128MJT125_EMIF_TIM2, .sdram_tim3 = MT41J128MJT125_EMIF_TIM3, .zq_config = MT41J128MJT125_ZQ_CFG, .emif_ddr_phy_ctlr_1 = MT41J128MJT125_EMIF_READ_LATENCY, }; #endif #if defined(CONFIG_NAND_OMAP_GPMC) & !defined(CONFIG_SPL_BUILD) /****************************************************************************** * OMAP3 specific command to switch between NAND HW and SW ecc *****************************************************************************/ static int do_switch_ecc(cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[]) { if (argc < 2) goto usage; if (strncmp(argv[1], "hw", 2) == 0) { int type = 1; if (argc == 3) type = simple_strtoul(argv[2], NULL, 10); omap_nand_switch_ecc(type); } else if (strncmp(argv[1], "sw", 2) == 0) omap_nand_switch_ecc(0); else goto usage; return 0; usage: printf ("Usage: nandecc %s\n", cmdtp->usage); return 1; } U_BOOT_CMD( nandecc, 3, 1, do_switch_ecc, "switch OMAP3 NAND ECC calculation algorithm", "[hw 1/hw 2/sw] - Switch between NAND ecc algorithm\n" " hw 1 = kernel/FS layout\n" " hw 2 = xloader/uboot layout\n" " sw = 1-bit software" ); #endif /* CONFIG_NAND_OMAP_GPMC & !CONFIG_SPL_BUILD */ /* * early system init of muxing and clocks. */ void s_init(void) { /* WDT1 is already running when the bootloader gets control * Disable it to avoid "random" resets */ writel(0xAAAA, &wdtimer->wdtwspr); while (readl(&wdtimer->wdtwwps) != 0x0) ; writel(0x5555, &wdtimer->wdtwspr); while (readl(&wdtimer->wdtwwps) != 0x0) ; #ifdef CONFIG_SPL_BUILD /* Setup the PLLs and the clocks for the peripherals */ pll_init(); /* Enable RTC32K clock */ rtc32k_enable(); /* UART softreset */ u32 regVal; regVal = readl(&uart_base->uartsyscfg); regVal |= UART_RESET; writel(regVal, &uart_base->uartsyscfg); while ((readl(&uart_base->uartsyssts) & UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK) ; /* Disable smart idle */ regVal = readl(&uart_base->uartsyscfg); regVal |= UART_SMART_IDLE_EN; writel(regVal, &uart_base->uartsyscfg); gd = &gdata; enable_board_pin_mux(); //gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en"); //gpio_direction_output(GPIO_DDR_VTT_EN, 1); preloader_console_init(); i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE); config_ddr(303, MT41J128MJT125_IOCTRL_VALUE, &ddr3_data, &ddr3_cmd_ctrl_data, &ddr3_emif_reg_data); #endif } /* * Basic board specific setup. Pinmux has been handled already. */ int board_init(void) { i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE); gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100; gpmc_init(); /* enable NAND flash chip select */ enable_gpmc_cs_config(gpmc_nand_config, &gpmc_cfg->cs[NAND_CS], NAND_BASE, NAND_SIZE); /* enable FRAM chip select */ enable_gpmc_cs_config(gpmc_fram_config, &gpmc_cfg->cs[FRAM_CS], FRAM_BASE, FRAM_SIZE); /* enable NOR flash chip select */ enable_gpmc_cs_config(gpmc_nor_config, &gpmc_cfg->cs[NOR_CS], NOR_BASE, NOR_SIZE); return 0; } #ifdef CONFIG_BOARD_LATE_INIT int board_late_init(void) { #ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG setenv("board_name", "NANOBONE"); setenv("board_rev", "0001"); #endif return 0; } #endif #ifdef CONFIG_DRIVER_TI_CPSW static void cpsw_control(int enabled) { /* VTP can be added here */ return; } static struct cpsw_slave_data cpsw_slaves[] = { { .slave_reg_ofs = 0x208, .sliver_reg_ofs = 0xd80, .phy_id = 0, }, { .slave_reg_ofs = 0x308, .sliver_reg_ofs = 0xdc0, .phy_id = 1, }, }; static struct cpsw_platform_data cpsw_data = { .mdio_base = AM335X_CPSW_MDIO_BASE, .cpsw_base = AM335X_CPSW_BASE, .mdio_div = 0xff, .channels = 8, .cpdma_reg_ofs = 0x800, .slaves = 1, .slave_data = cpsw_slaves, .ale_reg_ofs = 0xd00, .ale_entries = 1024, .host_port_reg_ofs = 0x108, .hw_stats_reg_ofs = 0x900, .mac_control = (1 << 5), .control = cpsw_control, .host_port_num = 0, .version = CPSW_CTRL_VERSION_2, }; #endif #if defined(CONFIG_DRIVER_TI_CPSW) || \ (defined(CONFIG_USB_ETHER) && defined(CONFIG_MUSB_GADGET)) int board_eth_init(bd_t *bis) { int rv, n = 0; #ifdef CONFIG_DRIVER_TI_CPSW uint8_t mac_addr[6]; uint32_t mac_hi, mac_lo; if (!eth_getenv_enetaddr("ethaddr", mac_addr)) { debug("<ethaddr> not set. Reading from E-fuse\n"); /* try reading mac address from efuse */ mac_lo = readl(&cdev->macid0l); mac_hi = readl(&cdev->macid0h); mac_addr[0] = mac_hi & 0xFF; mac_addr[1] = (mac_hi & 0xFF00) >> 8; mac_addr[2] = (mac_hi & 0xFF0000) >> 16; mac_addr[3] = (mac_hi & 0xFF000000) >> 24; mac_addr[4] = mac_lo & 0xFF; mac_addr[5] = (mac_lo & 0xFF00) >> 8; if (is_valid_ether_addr(mac_addr)) eth_setenv_enetaddr("ethaddr", mac_addr); else goto try_usbether; } writel(PORT1_MII_MODE_ENABLE | PORT2_RMII_MODE_ENABLE, &cdev->miisel); cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_MII; cpsw_slaves[1].phy_if = PHY_INTERFACE_MODE_RMII; rv = cpsw_register(&cpsw_data); if (rv < 0) printf("Error %d registering CPSW switch\n", rv); else n += rv; #endif try_usbether: #if defined(CONFIG_USB_ETHER) && !defined(CONFIG_SPL_BUILD) rv = usb_eth_initialize(bis); if (rv < 0) printf("Error %d registering USB_ETHER\n", rv); else n += rv; #endif return n; } #endif
/* * mux.c * * Copyright (C) 2013, Newflow Ltd - http://www.newflow.co.uk/ * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation version 2. * * This program is distributed "as is" WITHOUT ANY WARRANTY of any * kind, whether express or implied; without even the implied warranty * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. */ #include <common.h> #include <asm/arch/sys_proto.h> #include <asm/arch/hardware.h> #include <asm/arch/mux.h> #include <asm/io.h> #include <i2c.h> #include "board.h" static struct module_pin_mux gpmc_pin_mux[] = { {OFFSET(gpmc_ad0), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD0 */ {OFFSET(gpmc_ad1), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD1 */ {OFFSET(gpmc_ad2), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD2 */ {OFFSET(gpmc_ad3), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD3 */ {OFFSET(gpmc_ad4), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD4 */ {OFFSET(gpmc_ad5), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD5 */ {OFFSET(gpmc_ad6), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD6 */ {OFFSET(gpmc_ad7), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD7 */ {OFFSET(gpmc_ad8), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD8 */ {OFFSET(gpmc_ad9), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD9 */ {OFFSET(gpmc_ad10), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD10 */ {OFFSET(gpmc_ad11), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD11 */ {OFFSET(gpmc_ad12), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD12 */ {OFFSET(gpmc_ad13), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD13 */ {OFFSET(gpmc_ad14), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD14 */ {OFFSET(gpmc_ad15), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* GPMC AD15 */ {OFFSET(gpmc_csn0), (MODE(0) | PULLUDEN)}, /* GPMC_CSN0 */ {OFFSET(gpmc_csn1), (MODE(0) | PULLUDEN)}, /* GPMC_CSN1 */ {OFFSET(gpmc_csn2), (MODE(0) | PULLUDEN)}, /* GPMC_CSN2 */ {OFFSET(gpmc_csn3), (MODE(0) | PULLUDEN)}, /* GPMC_CSN3 */ {OFFSET(gpmc_advn_ale), (MODE(0) | PULLUDEN)}, /* GPMC_ADV_ALE */ {OFFSET(gpmc_oen_ren), (MODE(0) | PULLUDEN)}, /* GPMC_OE */ {OFFSET(gpmc_wen), (MODE(0) | PULLUDEN)}, /* GPMC_WEN */ {OFFSET(gpmc_be0n_cle), (MODE(0) | PULLUDEN)}, /* GPMC_BE_CLE */ {OFFSET(lcd_data1), (MODE(1) | PULLUDDIS)}, /* GPMC AD17 */ {OFFSET(lcd_data2), (MODE(1) | PULLUDDIS)}, /* GPMC AD18 */ {OFFSET(lcd_data3), (MODE(1) | PULLUDDIS)}, /* GPMC AD19 */ {OFFSET(lcd_data4), (MODE(1) | PULLUDDIS)}, /* GPMC AD20 */ {OFFSET(lcd_data5), (MODE(1) | PULLUDDIS)}, /* GPMC AD21 */ {OFFSET(lcd_data6), (MODE(1) | PULLUDDIS)}, /* GPMC AD22 */ {OFFSET(lcd_data7), (MODE(1) | PULLUDDIS)}, /* GPMC AD23 */ {OFFSET(lcd_data8), (MODE(1) | PULLUDDIS)}, /* GPMC AD24 */ {OFFSET(lcd_data9), (MODE(1) | PULLUDDIS)}, /* GPMC AD25 */ {OFFSET(lcd_data10), (MODE(1) | PULLUDDIS)}, /* GPMC AD26 */ {-1}, }; static struct module_pin_mux i2c0_pin_mux[] = { {OFFSET(i2c0_sda), (MODE(0) | RXACTIVE | PULLUDEN | SLEWCTRL)}, /* I2C_DATA */ {OFFSET(i2c0_scl), (MODE(0) | RXACTIVE | PULLUDEN | SLEWCTRL)}, /* I2C_SCLK */ {-1}, }; static struct module_pin_mux mii1_pin_mux[] = { {OFFSET(mii1_col), MODE(0) | RXACTIVE}, /* MII1_COL */ {OFFSET(mii1_crs), MODE(0) | RXACTIVE}, /* MII1_CRS */ {OFFSET(mii1_rxerr), MODE(0) | RXACTIVE}, /* MII1_RXERR */ {OFFSET(mii1_txen), MODE(0)}, /* MII1_TXEN */ {OFFSET(mii1_rxdv), MODE(0) | RXACTIVE}, /* MII1_RXDV */ {OFFSET(mii1_txd3), MODE(0)}, /* MII1_TXD3 */ {OFFSET(mii1_txd2), MODE(0)}, /* MII1_TXD2 */ {OFFSET(mii1_txd1), MODE(0)}, /* MII1_TXD1 */ {OFFSET(mii1_txd0), MODE(0)}, /* MII1_TXD0 */ {OFFSET(mii1_txclk), MODE(0) | RXACTIVE}, /* MII1_TXCLK */ {OFFSET(mii1_rxclk), MODE(0) | RXACTIVE}, /* MII1_RXCLK */ {OFFSET(mii1_rxd3), MODE(0) | RXACTIVE}, /* MII1_RXD3 */ {OFFSET(mii1_rxd2), MODE(0) | RXACTIVE}, /* MII1_RXD2 */ {OFFSET(mii1_rxd1), MODE(0) | RXACTIVE}, /* MII1_RXD1 */ {OFFSET(mii1_rxd0), MODE(0) | RXACTIVE}, /* MII1_RXD0 */ {OFFSET(mdio_data), MODE(0) | RXACTIVE | PULLUP_EN}, /* MDIO_DATA */ {OFFSET(mdio_clk), MODE(0) | PULLUP_EN}, /* MDIO_CLK */ {-1}, }; static struct module_pin_mux mii2_pin_mux[] = { {OFFSET(gpmc_a0), MODE(1)}, /* MII2_TXEN */ {OFFSET(gpmc_a1), MODE(1) | RXACTIVE}, /* MII2_RXDV */ {OFFSET(gpmc_a2), MODE(1)}, /* MII2_TXD3 */ {OFFSET(gpmc_a3), MODE(1)}, /* MII2_TXD2 */ {OFFSET(gpmc_a4), MODE(1)}, /* MII2_TXD1 */ {OFFSET(gpmc_a5), MODE(1)}, /* MII2_TXD0 */ {OFFSET(gpmc_a6), MODE(1) | RXACTIVE}, /* MII2_TXCLK */ {OFFSET(gpmc_a7), MODE(1) | RXACTIVE}, /* MII2_RXCLK */ {OFFSET(gpmc_a8), MODE(1) | RXACTIVE}, /* MII2_RXD3 */ {OFFSET(gpmc_a9), MODE(1) | RXACTIVE}, /* MII2_RXD2 */ {OFFSET(gpmc_a10), MODE(1) | RXACTIVE}, /* MII2_RXD1 */ {OFFSET(gpmc_a11), MODE(1) | RXACTIVE}, /* MII2_RXD0 */ {OFFSET(gpmc_wait0), MODE(1) | RXACTIVE}, /* MII2_CRS */ {OFFSET(gpmc_wpn), MODE(1) | RXACTIVE}, /* MII2_RXERR */ {OFFSET(gpmc_be1n), MODE(1) | RXACTIVE}, /* MII2_COL */ {OFFSET(mdio_data), MODE(0) | RXACTIVE | PULLUP_EN}, /* MDIO_DATA */ {OFFSET(mdio_clk), MODE(0) | PULLUP_EN}, /* MDIO_CLK */ // CRS/BSY_SEL //{OFFSET(spi0_cs0), (MODE(7) | PULLUDEN)}, /* GPIO0_5 */ {-1}, }; static struct module_pin_mux mmc0_no_cd_pin_mux[] = { {OFFSET(mmc0_dat3), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_DAT3 */ {OFFSET(mmc0_dat2), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_DAT2 */ {OFFSET(mmc0_dat1), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_DAT1 */ {OFFSET(mmc0_dat0), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_DAT0 */ {OFFSET(mmc0_clk), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_CLK */ {OFFSET(mmc0_cmd), (MODE(0) | RXACTIVE | PULLUP_EN)}, /* MMC0_CMD */ {OFFSET(mcasp0_aclkr), (MODE(4) | RXACTIVE)}, /* MMC0_WP */ {OFFSET(emu1), (MODE(7) | RXACTIVE)}, /* MMC0_CD */ //{OFFSET(mcasp0_fsr), (MODE(7))}, /* MMC0_PWR */ {-1}, }; static struct module_pin_mux rmii1_pin_mux[] = { {OFFSET(mii1_crs), MODE(1) | RXACTIVE}, /* RMII1_CRS_DV */ {OFFSET(mii1_rxerr), MODE(1) | RXACTIVE}, /* RMII1_RXER */ {OFFSET(mii1_txen), MODE(1)}, /* RMII1_TXEN */ {OFFSET(mii1_txd1), MODE(1)}, /* RMII1_TXD1 */ {OFFSET(mii1_txd0), MODE(1)}, /* RMII1_TXD0 */ {OFFSET(mii1_rxd1), MODE(1) | RXACTIVE}, /* RMII1_RXD1 */ {OFFSET(mii1_rxd0), MODE(1) | RXACTIVE}, /* RMII1_RXD0 */ {OFFSET(mdio_data), MODE(0) | RXACTIVE | PULLUP_EN},/* MDIO_DATA */ {OFFSET(mdio_clk), MODE(0) | PULLUP_EN}, /* MDIO_CLK */ {-1}, }; static struct module_pin_mux rmii2_pin_mux[] = { {OFFSET(gpmc_wait0), MODE(3) | RXACTIVE}, /* RMII2_CRS_DV */ {OFFSET(gpmc_wpn), MODE(3) | RXACTIVE}, /* RMII2_RXER */ {OFFSET(gpmc_a0), MODE(3)}, /* RMII2_TXEN */ {OFFSET(gpmc_a4), MODE(3)}, /* RMII2_TXD1 */ {OFFSET(gpmc_a5), MODE(3)}, /* RMII2_TXD0 */ {OFFSET(gpmc_a10), MODE(3) | RXACTIVE}, /* RMII2_RXD1 */ {OFFSET(gpmc_a11), MODE(3) | RXACTIVE}, /* RMII2_RXD0 */ {OFFSET(mdio_data), MODE(0) | RXACTIVE | PULLUP_EN},/* MDIO_DATA */ {OFFSET(mdio_clk), MODE(0) | PULLUP_EN}, /* MDIO_CLK */ {-1}, }; static struct module_pin_mux uart0_pin_mux[] = { {OFFSET(uart0_rxd), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* UART0_RXD */ {OFFSET(uart0_txd), (MODE(0) | PULLUDEN)}, /* UART0_TXD */ {-1}, }; static struct module_pin_mux uart1_pin_mux[] = { {OFFSET(uart1_ctsn), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* UART1_CTSN */ {OFFSET(uart1_rtsn), (MODE(0) | PULLUDEN)}, /* UART1_RTSN */ {OFFSET(uart1_rxd), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* UART1_RXD */ {OFFSET(uart1_txd), (MODE(0) | PULLUDEN)}, /* UART1_TXD */ {-1}, }; static struct module_pin_mux uart2_pin_mux[] = { {OFFSET(lcd_data8), (MODE(6) | PULLUP_EN | RXACTIVE)}, /* UART2_CTSN */ {OFFSET(lcd_data9), (MODE(6) | PULLUDEN)}, /* UART2_RTSN */ {OFFSET(spi0_sclk), (MODE(1) | PULLUP_EN | RXACTIVE)}, /* UART2_RXD */ {OFFSET(spi0_d0), (MODE(1) | PULLUDEN)}, /* UART2_TXD */ {-1}, }; static struct module_pin_mux uart3_pin_mux[] = { {OFFSET(lcd_data10), (MODE(6) | PULLUP_EN | RXACTIVE)}, /* UART3_CTSN */ {OFFSET(lcd_data11), (MODE(6) | PULLUDEN)}, /* UART3_RTSN */ {OFFSET(spi0_cs1), (MODE(1) | PULLUP_EN | RXACTIVE)}, /* UART3_RXD */ {OFFSET(ecap0_in_pwm0_out), (MODE(1) | PULLUDEN)}, /* UART3_TXD */ {-1}, }; static struct module_pin_mux uart4_pin_mux[] = { {OFFSET(lcd_data12), (MODE(6) | PULLUP_EN | RXACTIVE)}, /* UART4_CTSN */ {OFFSET(lcd_data13), (MODE(6) | PULLUDEN)}, /* UART4_RTSN */ {OFFSET(uart0_ctsn), (MODE(1) | PULLUP_EN | RXACTIVE)}, /* UART4_RXD */ {OFFSET(uart0_rtsn), (MODE(1) | PULLUDEN)}, /* UART4_TXD */ {-1}, }; static struct module_pin_mux uart5_pin_mux[] = { {OFFSET(lcd_data14), (MODE(4) | PULLUP_EN | RXACTIVE)}, /* UART5_RXD */ {OFFSET(rmii1_refclk), (MODE(3) | PULLUDEN)}, /* UART5_TXD */ {-1}, }; static struct module_pin_mux usb0_pin_mux[] = { {OFFSET(usb0_dm), (MODE(0) | RXACTIVE)}, /* USB0_DM */ {OFFSET(usb0_dp), (MODE(0) | RXACTIVE)}, /* USB0_DP */ {OFFSET(usb0_ce), (MODE(0) | RXACTIVE)}, /* USB0_CE */ {OFFSET(usb0_id), (MODE(0) | RXACTIVE)}, /* USB0_ID */ {OFFSET(usb0_vbus), (MODE(0) | RXACTIVE)}, /* USB0_VBUS */ {OFFSET(usb0_drvvbus), (MODE(0) | PULLUDEN)}, /* USB0_DRVVBUS */ {-1}, }; static struct module_pin_mux usb1_pin_mux[] = { {OFFSET(usb1_dm), (MODE(0) | RXACTIVE)}, /* USB1_DM */ {OFFSET(usb1_dp), (MODE(0) | RXACTIVE)}, /* USB1_DP */ {OFFSET(usb1_ce), (MODE(0) | RXACTIVE)}, /* USB1_CE */ {OFFSET(usb1_id), (MODE(0) | RXACTIVE)}, /* USB1_ID */ {OFFSET(usb1_vbus), (MODE(0) | RXACTIVE)}, /* USB1_VBUS */ {OFFSET(usb1_drvvbus), (MODE(0) | PULLUDEN)}, /* USB1_DRVVBUS */ {-1}, }; void enable_board_pin_mux() { configure_module_pin_mux(gpmc_pin_mux); configure_module_pin_mux(i2c0_pin_mux); configure_module_pin_mux(mii1_pin_mux); //configure_module_pin_mux(rmii2_pin_mux); configure_module_pin_mux(mmc0_no_cd_pin_mux); configure_module_pin_mux(uart0_pin_mux); configure_module_pin_mux(uart1_pin_mux); configure_module_pin_mux(uart2_pin_mux); configure_module_pin_mux(uart3_pin_mux); configure_module_pin_mux(uart4_pin_mux); configure_module_pin_mux(uart5_pin_mux); configure_module_pin_mux(usb0_pin_mux); configure_module_pin_mux(usb1_pin_mux); }