Hi,
Can DM816x encode to, and decode video from, the following video resolutions?
- NTSC: 720 x 480 resolution, selectable 4:3 or 16:9 aspect ratio, 29.97 frames/sec, interlaced
- PAL: 720 x 576 resolution, selectable 4:3 or 16:9 aspect ratio, 25 frames/sec, interlaced
- RGB: up to 1600 x 1200 resolution, up to 60 frames/sec, non-interlaced
Thanks