This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compliance of the MMC ports on AM3352

Guru 16800 points
Other Parts Discussed in Thread: AM3352, CSD

Hi,

I'm using AM3352.
I find that the AM3352's MMC ports comply with MMC4.3, which is described in datasheet.
However, I want to use MMC complied with MMC4.5.
Is it possible?

If the differences between MMC4.3 and MMC4.5 are only software (device drivers),
I think that AM3352's MMC ports can comply with MMC4.3.
However, if the modifications of hardware are needed, it is impossible, I think.
I'm sorry, but I don't know the differences between MMC4.3 and MMC4.5.

Thanks

Nomoto