This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using AM3352.
I find that the AM3352's MMC ports comply with MMC4.3, which is described in datasheet.
However, I want to use MMC complied with MMC4.5.
Is it possible?
If the differences between MMC4.3 and MMC4.5 are only software (device drivers),
I think that AM3352's MMC ports can comply with MMC4.3.
However, if the modifications of hardware are needed, it is impossible, I think.
I'm sorry, but I don't know the differences between MMC4.3 and MMC4.5.
Thanks
Nomoto