Other Parts Discussed in Thread: AM3352
Hi,
I am using AM3352 and released SDK for AM3352 (version 5.06).
The "ti-sdk-am335x-evm-05.06.00.00/board-support/linux-3.2.0-psp05.06.00.00/patches" directory includes the divided kernel patches, I think.
Could you teach me a difference between "the kernel which should be put the above divided kernel patches" and Kernel 3.2?
Briefly, I want to know the differences between Kernel in SDK and Kernel 3.2.
I thought that I should apply the above patches to Kernel 3.2, however it is impossible, because "0001-musb-update ..." cannot be applied to Kernel 3.2.
It is difficult to extract the divided patches from the Git repository included in the "ti-sdk-am335x-evm-05.06.00.00/board-support/board-port-labs/sitara-board-port-linux" directory.
Thanks
Nomoto