This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 FIRMWARE: Memory map bin file not passed

Other Parts Discussed in Thread: SYSCONFIG

Hello,

I use the ezsdk_dm814x-evm_5_05_02_00 ,when I use the ezsdk-dm814x-evm-rootfs as the rootfs

some error appeared.The kernel log is:

PRCM Initialization completed
SysLink version : 2.20.02.20
SysLink module created on Date:Mar 20 2013 Time:14:48:52
PM: Adding info for No Bus:syslinkipc_Osal
PM: Adding info for No Bus:syslinkipc_Ipc
PM: Adding info for No Bus:syslinkipc_ProcMgr
PM: Adding info for No Bus:syslinkipc_Notify
PM: Adding info for No Bus:syslinkipc_MultiProc
PM: Adding info for No Bus:syslinkipc_NameServer
PM: Adding info for No Bus:syslinkipc_SharedRegion
PM: Adding info for No Bus:syslinkipc_HeapBufMP
PM: Adding info for No Bus:syslinkipc_HeapMemMP
PM: Adding info for No Bus:syslinkipc_ListMP
PM: Adding info for No Bus:syslinkipc_GateMP
PM: Adding info for No Bus:syslinkipc_MessageQ
PM: Adding info for No Bus:syslinkipc_SyslinkMemMgr
PM: Adding info for No Bus:syslinkipc_ClientNotifyMgr
PM: Adding info for No Bus:syslinkipc_FrameQBufMgr
PM: Adding info for No Bus:syslinkipc_FrameQ
PM: Adding info for No Bus:syslinkipc_RingIO
PM: Adding info for No Bus:syslinkipc_RingIOShm
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 1 start Successful
Loading HDVPSS Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 2 start Successful
VPSS_FVID2: M3 firmware version 0x1000145 is newer,driver may not work properly.
PM: Adding info for No Bus:fb0
PM: Adding info for No Bus:fb1
PM: Adding info for No Bus:fb2
Configuring fb0 to LCD
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
PM: Adding info for No Bus:TI81XX_HDMI
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 1
hdmi: *** Set PHY power mode to 2
I2C No Ack

HDMI failed to read E-EDID
hdmi: Enter HDMI_W1_GlobalInitVars()
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame ()
hdmi: Irqenable 60000011
hdmi: 40 hpd
hdmi: -------------DEBUG-------------------
hdmi: 1 hdmi_wp_irqstatus
hdmi: 1 hdmi_core_intr_state
hdmi: 40 hdmi_core_intr1
hdmi: 3 hdmi_core_intr2
hdmi: 9 hdmi_core_intr3
hdmi: 83 hdmi_core_sys_sys_stat
hdmi: -------------DEBUG-------------------
hdmi: first hpd
PM: Adding info for No Bus:tlc59108-bl
Starting system message bus: dbus.
Starting Dropbear SSH server: NET: Registered protocol family 10
dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
PVR: PVRCore_Init
PM: Adding info for platform:pvrsrvkm
PVR: PVRSRVDriverProbe(pDevice=bf21d140)
PVR: EnableSystemClocks: Enabling System Clocks
PVR: GPTIMER11 clock is 20MHz
PVR: OSUnMapPhysToLin: unmapping 4 bytes from fa048054
PVR: OSUnMapPhysToLin: unmapping 4 bytes from fa048038
PVR: PVRCore_Init: major device 250
PM: Adding info for No Bus:pvrsrvkm
PM: Adding info for No Bus:bccat0
/dev/mem opened.
Memory mapped at address 0x4027e000.
Read at address 0x48180F04 (0x4027ef04): 0x00000001
Write at address 0x48180F04 (0x4027ef04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x40284000.
Read at address 0x48180900 (0x40284900): 0x00000102
Write at address 0x48180900 (0x40284900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x40314000.
Read at address 0x48180920 (0x40314920): 0x00040002
Write at address 0x48180920 (0x40314920): 0x00000002, readback 0x00000002
PVR: Installing MISR with cookie bf21e81c
PVR: Installing device LISR SGX ISR on IRQ 37 with cookie ca077f00
PVR: OSUnMapPhysToLin: unmapping 65536 bytes from d5ba0000
PVR_K:(Warning): SysFinalise: Version string: SGX revision = 1.2.5 [583, usr/local/ezsdk02/component-sources/graphics-sdk_4.04.00.02/GFX_Linux_KM/services4/system/ti81xx/sysconfig.c]
PVR_K: (FAIL) SGXInit: Mismatch in client-side and KM driver build options; extra options present in KM: (0x1). Please check sgx_options.h
PVR_K:(Error): PVRSRVFinaliseSystem: Failed PVRSRVDevInitCompatCheck call (device index: 0) [422, usr/local/ezsdk02/component-sources/graphics-sdk_4.04.00.02/GFX_Linux_KM/services4/srvkm/common/pvrsrv.c]
PVR_K:(Error): BridgedDispatchKM: Initialisation failed. Driver unusable. [3785, usr/local/ezsdk02/component-sources/graphics-sdk_4.04.00.02/GFX_Linux_KM/services4/srvkm/bridged/bridged_pvr_bridge.c]
Calibrating touchscreen (first time only)ts_open: No such file or directory
.
Starting Matrix GUI application.

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org dm814x-evm ttyO0

Arago 2011.09 dm814x-evm ttyO0

dm814x-evm login: eth0: no IPv6 routers present
root
root@dm814x-evm:~#

I don't know what is the reason of this error.

thanks

Enson