This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
First boot of Kernel and file system OK.
Second boot U-Boot has multiple ECC errors at offset 6c0000.
Third boot U-Boot has multiple ECC errors at offset 6c0000 and kernel crashes.
Anyone have this problem with booting UBIFS from NAND Flash multiple times?
John
------------------------------------------------------------------------------------------------------------
------------------------------ First Boot from NAND Flash ---------------------------------------
------------------------------------------------------------------------------------------------------------
NAND read: device 0 offset 0x280000, size 0x240000
2359296 bytes read: OK
NAND read: device 0 offset 0x6c0000, size 0x5800000
92274688 bytes read: OK
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2310980 Bytes = 2.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (jwilly@aeon) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #57 Fri Mar 22 16:34:13 PDT 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.1
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648
Kernel command line: console=ttyO0,115200n8 rootdelay=5 noinitrd rw mem=364M@0x80000000 mem=320M@0x9fc00000 vmalloc=500M notifyk.vpssm3_sva=0xbf900000 ubi.mtd=4,2048 rootfstype=ubifs root=ubi0:rootfs init=/init ip=192.168.1.177:192.168.1.188:192.168.1.16:255.255.255.0:kiwidev:eth0:off
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 364MB 270MB = 634MB total
Memory: 638340k/638340k available, 62076k reserved, 276480K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB)
lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0037000 ( 188 kB)
.text : 0xc0037000 - 0xc045c000 (4244 kB)
.data : 0xc045c000 - 0xc049b900 ( 255 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
omap_hwmod: gpio1: softreset failed (waited 10000 usec)
omap_hwmod: gpio2: softreset failed (waited 10000 usec)
omap_hwmod: gpio3: softreset failed (waited 10000 usec)
omap_hwmod: gpio4: softreset failed (waited 10000 usec)
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 719.25 BogoMIPS (lpj=3596288)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
Kernel (board-ti8148evm.c) Start
ti81xx_register_mcasp mcasp0
ti81xx_register_mcasp mcasp1
ti81xx_register_mcasp mcasp2 setting mcasp2_ahclkx to output
NOR: Can't request GPMC CS
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:01:00.0: BAR 1: assigned [mem 0x20000000-0x2000ffff]
pci 0000:01:00.0: BAR 1: set to [mem 0x20000000-0x2000ffff] (PCI address [0x20000000-0x2000ffff])
pci 0000:01:00.0: BAR 2: assigned [mem 0x20010000-0x2001ffff]
pci 0000:01:00.0: BAR 2: set to [mem 0x20010000-0x2001ffff] (PCI address [0x20010000-0x2001ffff])
pci 0000:01:00.0: BAR 3: assigned [mem 0x20020000-0x20021fff]
pci 0000:01:00.0: BAR 3: set to [mem 0x20020000-0x20021fff] (PCI address [0x20020000-0x20021fff])
pci 0000:01:00.0: BAR 0: assigned [mem 0x20022000-0x20022fff]
pci 0000:01:00.0: BAR 0: set to [mem 0x20022000-0x20022fff] (PCI address [0x20022000-0x20022fff])
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 706
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
omap2-nand driver initializing
ONFI param page 0 valid
ONFI flash detected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)
omap2-nand: detected x16 NAND flash
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000020000000 : "Reserved"
UBI: attaching mtd4 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: sub-page size: 512
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI: max. sequence number: 0
UBI: volume 0 ("rootfs") re-sized from 826 to 1581 LEBs
UBI: attached mtd4 to ubi0
UBI: MTD device name: "File System"
UBI: MTD device size: 200 MiB
UBI: number of good PEBs: 1601
UBI: number of bad PEBs: 0
UBI: number of corrupted PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 1601
UBI: number of PEBs reserved for bad PEB handling: 16
UBI: max/mean erase counter: 1/0
UBI: image sequence number: 68837352
UBI: background thread "ubi_bgt0d" started, PID 36
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
d_can d_can: d_can device registered (irq=52, irq_obj=53)
mice: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=0:17:eb:50:e0:d6
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
>>>> phy_connect:bus id 0:00<<<<
CPSW phy found : id is : 0x221611
>>>>cpsw_set_phy_config <<<<
>>>>cpsw_set_phy_config: Link Status 796d <<<<
IP-Config: Complete:
device=eth0, addr=192.168.1.177, mask=255.255.255.0, gw=192.168.1.16,
host=kiwidev, domain=, nis-domain=(none),
bootserver=192.168.1.188, rootserver=192.168.1.188, rootpath=
Waiting 5sec before mounting root device...
PHY: 0:00 - Link is Up - 1000/Full
UBIFS: mounted UBI device 0, volume 0, name "rootfs"
UBIFS: file system size: 199352320 bytes (194680 KiB, 190 MiB, 1570 LEBs)
UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
UBIFS: media format: w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root: 0 bytes (0 KiB)
VFS: Mounted root (ubifs filesystem) on device 0:13.
devtmpfs: mounted
Freeing init memory: 188K
Failed to execute /init. Attempting defaults...
INIT: version 2.86 booting
/etc/rcS.d/S01psplash: line 16: machine_id: not found
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
udevd (67): /proc/67/oom_adj is deprecated, please use /proc/67/oom_score_adj instead.
dvm_pci_driver: initialising
revision:0:wait queue test: dev->dev.kobj.name: "0000:01:00.0"
PCI BAR0: 20022000 : bar0_len: 00001000
PCI BAR0 remap: d71d6000
PCI BAR1: 20000000 : bar1_len: 00010000
PCI BAR1 remap: d71e0000
PCI BAR2: 20010000 : bar2_len: 00010000
PCI BAR2 remap: d7200000
PCI BAR3: 20020000 : bar3_len: 00002000
PCI BAR3 remap: d71dc000
0000:01:00.0: Memory Allocated: ffc00000 DMA Address: 95e00000
PCI: enabling device 0000:01:00.0 (0144 -> 0146)
dvm_pci_probe: IRQ 48.
dvm_pci_driver: major dev 231:
Root filesystem already rw, not remounting
Caching udev devnodes
NET: Registered protocol family 10
logger: mount: mount point /proc/bus/usb does not exist
ALSA: Restoring mixer settings...
Configuring network interfaces... done.
Setting up IP spoofing protection: rp_filter.
/usr/sbin/alsactl: load_state:1625: No soundcards found...
Fri Jun 8 19:21:00 UTC 2012
INIT: Entering runlevel: 5
Adding /dev/hdmi_cntl to /dev
Adding /dev/gpio_cntl to /dev
Adding /dev/dvm_fpgaflash to /dev
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000001
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00050002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x3a760475
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0xc81df502
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM Initialization completed
SysLink version : 2.10.03.20
SysLink module created on Date:Apr 30 2012 Time:01:23:00
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS (V4L2) Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 0
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
Configuring fb0 to LCD
gpio_cntl_init : Major number 125
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:480 height:272
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:480 height:272
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:720 height:480
ti81xxvin_probe: v4l2_device_register 0
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 0
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 4c
ti81xxvin_probe:v4l2_i2c_new_subdev_board type adv7611
ti81xxvin_probe:v4l2_i2c_new_subdev_board d5c4d080
adv7611 probe
adv7611 1-004c: adv7611_probe: adv7611_state created
adv7611 1-004c: adv7611 found @ 0x4c (OMAP I2C adapter)
adv7611 1-004c: Rev. 2051 detected.
ti81xxvin ti81xxvin: registered sub device adv7611
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 1
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 10
ti81xxvin_probe:v4l2_i2c_new_subdev_board type dvmsdia
ti81xxvin_probe:v4l2_i2c_new_subdev_board 73656369
ti81xxvin ti81xxvin: registered sub device dvm-sdi-a
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 2
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 12
ti81xxvin_probe:v4l2_i2c_new_subdev_board type dvmsdib
ti81xxvin_probe:v4l2_i2c_new_subdev_board 7269762f
ti81xxvin ti81xxvin: registered sub device dvm-sdi-b
ti81xxvin ti81xxvin: TI81xx HDVPSS Capture driver initialized
---- dvm_vmpp_audio_init ---- OSC_SRC) 00000000
---- dvm_vmpp_audio_init ---- OSC_SRC) 01000000
---- dvm_vmpp_audio_init ---- AUDIO_PLLCLKCNTL) 0791080e
---- dvm_vmpp_audio_init ---- MCASP2_CLKSEL) 00000002
---- dvm_vmpp_audio_init ---- MCASP2_CLKSEL) 00000000
dvm_vmpp_audio_probe
dvm_snd_soc_read: reg: 24
asoc: dvm-audio-dai <-> davinci-mcasp.2 mapping ok
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
dm814x-dvm login:
------------------------------------------------------------------------------------------------------------
------------------------------ Second Boot from NAND Flash ---------------------------------------
------------------------------------------------------------------------------------------------------------
NAND read: device 0 offset 0x280000, size 0x240000
2359296 bytes read: OK
NAND read: device 0 offset 0x6c0000, size 0x5800000
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
NAND read from offset 6c0000 failed -74
92274688 bytes read: ERROR
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2310980 Bytes = 2.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (jwilly@aeon) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #57 Fri Mar 22 16:34:13 PDT 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.1
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648
Kernel command line: console=ttyO0,115200n8 rootdelay=5 noinitrd rw mem=364M@0x80000000 mem=320M@0x9fc00000 vmalloc=500M notifyk.vpssm3_sva=0xbf900000 ubi.mtd=4,2048 rootfstype=ubifs root=ubi0:rootfs init=/init ip=192.168.1.177:192.168.1.188:192.168.1.16:255.255.255.0:kiwidev:eth0:off
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 364MB 270MB = 634MB total
Memory: 638340k/638340k available, 62076k reserved, 276480K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB)
lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0037000 ( 188 kB)
.text : 0xc0037000 - 0xc045c000 (4244 kB)
.data : 0xc045c000 - 0xc049b900 ( 255 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
omap_hwmod: gpio1: softreset failed (waited 10000 usec)
omap_hwmod: gpio2: softreset failed (waited 10000 usec)
omap_hwmod: gpio3: softreset failed (waited 10000 usec)
omap_hwmod: gpio4: softreset failed (waited 10000 usec)
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 719.25 BogoMIPS (lpj=3596288)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
Kernel (board-ti8148evm.c) Start
ti81xx_register_mcasp mcasp0
ti81xx_register_mcasp mcasp1
ti81xx_register_mcasp mcasp2 setting mcasp2_ahclkx to output
NOR: Can't request GPMC CS
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:01:00.0: BAR 1: assigned [mem 0x20000000-0x2000ffff]
pci 0000:01:00.0: BAR 1: set to [mem 0x20000000-0x2000ffff] (PCI address [0x20000000-0x2000ffff])
pci 0000:01:00.0: BAR 2: assigned [mem 0x20010000-0x2001ffff]
pci 0000:01:00.0: BAR 2: set to [mem 0x20010000-0x2001ffff] (PCI address [0x20010000-0x2001ffff])
pci 0000:01:00.0: BAR 3: assigned [mem 0x20020000-0x20021fff]
pci 0000:01:00.0: BAR 3: set to [mem 0x20020000-0x20021fff] (PCI address [0x20020000-0x20021fff])
pci 0000:01:00.0: BAR 0: assigned [mem 0x20022000-0x20022fff]
pci 0000:01:00.0: BAR 0: set to [mem 0x20022000-0x20022fff] (PCI address [0x20022000-0x20022fff])
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 706
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
omap2-nand driver initializing
ONFI param page 0 valid
ONFI flash detected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)
omap2-nand: detected x16 NAND flash
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000020000000 : "Reserved"
UBI: attaching mtd4 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: sub-page size: 512
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI: max. sequence number: 3
UBI: attached mtd4 to ubi0
UBI: MTD device name: "File System"
UBI: MTD device size: 200 MiB
UBI: number of good PEBs: 1601
UBI: number of bad PEBs: 0
UBI: number of corrupted PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 1601
UBI: number of PEBs reserved for bad PEB handling: 16
UBI: max/mean erase counter: 1/0
UBI: image sequence number: 68837352
UBI: background thread "ubi_bgt0d" started, PID 36
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
CAN device driver interface
CAN bus driver for Bosch
Root filesystem already rw, not remounting
Caching udev devnodes
NET: Registered protocol family 10
logger: mount: mount point /proc/bus/usb does not exist
ALSA: Restoring mixer settings...
Configuring network interfaces... done.
Setting up IP spoofing protection: rp_filter.
/usr/sbin/alsactl: load_state:1625: No soundcards found...
Fri Jun 8 19:21:00 UTC 2012
INIT: Entering runlevel: 5
Adding /dev/hdmi_cntl to /dev
Adding /dev/gpio_cntl to /dev
Adding /dev/dvm_fpgaflash to /dev
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000001
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00050002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x3a76046f
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0xc81df502
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM Initialization completed
SysLink version : 2.10.03.20
SysLink module created on Date:Apr 30 2012 Time:01:23:00
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS (V4L2) Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 0
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
Configuring fb0 to LCD
gpio_cntl_init : Major number 125
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:480 height:272
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:480 height:272
ti81xxvid_setup_video width:0 height:0
ti81xxvid_setup_video width:720 height:480
ti81xxvin_probe: v4l2_device_register 0
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 0
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 4c
ti81xxvin_probe:v4l2_i2c_new_subdev_board type adv7611
ti81xxvin_probe:v4l2_i2c_new_subdev_board d67d6080
adv7611 probe
adv7611 1-004c: adv7611_probe: adv7611_state created
adv7611 1-004c: adv7611 found @ 0x4c (OMAP I2C adapter)
adv7611 1-004c: Rev. 2051 detected.
ti81xxvin ti81xxvin: registered sub device adv7611
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 1
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 10
ti81xxvin_probe:v4l2_i2c_new_subdev_board type dvmsdia
ti81xxvin_probe:v4l2_i2c_new_subdev_board 73656369
ti81xxvin ti81xxvin: registered sub device dvm-sdi-a
ti81xxvin_probe:v4l2_i2c_new_subdev_board instance 2
ti81xxvin_probe:v4l2_i2c_new_subdev_board I2C addr 12
ti81xxvin_probe:v4l2_i2c_new_subdev_board type dvmsdib
ti81xxvin_probe:v4l2_i2c_new_subdev_board 7269762f
ti81xxvin ti81xxvin: registered sub device dvm-sdi-b
ti81xxvin ti81xxvin: TI81xx HDVPSS Capture driver initialized
---- dvm_vmpp_audio_init ---- OSC_SRC) 00000000
---- dvm_vmpp_audio_init ---- OSC_SRC) 01000000
---- dvm_vmpp_audio_init ---- AUDIO_PLLCLKCNTL) 0791080e
---- dvm_vmpp_audio_init ---- MCASP2_CLKSEL) 00000002
---- dvm_vmpp_audio_init ---- MCASP2_CLKSEL) 00000000
dvm_vmpp_audio_probe
dvm_snd_soc_read: reg: 24
asoc: dvm-audio-dai <-> davinci-mcasp.2 mapping ok
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
dm814x-dvm login:
------------------------------------------------------------------------------------------------------------
------------------------------ Third Boot Boot from NAND Flash ---------------------------------------
------------------------------------------------------------------------------------------------------------
NAND read: device 0 offset 0x280000, size 0x240000
2359296 bytes read: OK
NAND read: device 0 offset 0x6c0000, size 0x5800000
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
ECC: uncorrectable.
NAND read from offset 6c0000 failed -74
92274688 bytes read: ERROR
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2310980 Bytes = 2.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (jwilly@aeon) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #57 Fri Mar 22 16:34:13 PDT 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.1
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648
Kernel command line: console=ttyO0,115200n8 rootdelay=5 noinitrd rw mem=364M@0x80000000 mem=320M@0x9fc00000 vmalloc=500M notifyk.vpssm3_sva=0xbf900000 ubi.mtd=4,2048 rootfstype=ubifs root=ubi0:rootfs init=/init ip=192.168.1.177:192.168.1.188:192.168.1.16:255.255.255.0:kiwidev:eth0:off
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 364MB 270MB = 634MB total
Memory: 638340k/638340k available, 62076k reserved, 276480K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB)
lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0037000 ( 188 kB)
.text : 0xc0037000 - 0xc045c000 (4244 kB)
.data : 0xc045c000 - 0xc049b900 ( 255 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
omap_hwmod: gpio1: softreset failed (waited 10000 usec)
omap_hwmod: gpio2: softreset failed (waited 10000 usec)
omap_hwmod: gpio3: softreset failed (waited 10000 usec)
omap_hwmod: gpio4: softreset failed (waited 10000 usec)
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 719.25 BogoMIPS (lpj=3596288)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
Kernel (board-ti8148evm.c) Start
ti81xx_register_mcasp mcasp0
ti81xx_register_mcasp mcasp1
ti81xx_register_mcasp mcasp2 setting mcasp2_ahclkx to output
NOR: Can't request GPMC CS
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x20000000-0x200fffff]
pci 0000:01:00.0: BAR 1: assigned [mem 0x20000000-0x2000ffff]
pci 0000:01:00.0: BAR 1: set to [mem 0x20000000-0x2000ffff] (PCI address [0x20000000-0x2000ffff])
pci 0000:01:00.0: BAR 2: assigned [mem 0x20010000-0x2001ffff]
pci 0000:01:00.0: BAR 2: set to [mem 0x20010000-0x2001ffff] (PCI address [0x20010000-0x2001ffff])
pci 0000:01:00.0: BAR 3: assigned [mem 0x20020000-0x20021fff]
pci 0000:01:00.0: BAR 3: set to [mem 0x20020000-0x20021fff] (PCI address [0x20020000-0x20021fff])
pci 0000:01:00.0: BAR 0: assigned [mem 0x20022000-0x20022fff]
pci 0000:01:00.0: BAR 0: set to [mem 0x20022000-0x20022fff] (PCI address [0x20022000-0x20022fff])
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x20000000-0x200fffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 706
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
omap2-nand driver initializing
ONFI param page 0 valid
ONFI flash detected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)
omap2-nand: detected x16 NAND flash
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000020000000 : "Reserved"
UBI: attaching mtd4 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: sub-page size: 512
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI: max. sequence number: 7
UBI: attached mtd4 to ubi0
UBI: MTD device name: "File System"
UBI: MTD device size: 200 MiB
UBI: number of good PEBs: 1601
UBI: number of bad PEBs: 0
UBI: number of corrupted PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 1601
UBI: number of PEBs reserved for bad PEB handling: 16
UBI: max/mean erase counter: 2/0
UBI: image sequence number: 68837352
UBI: background thread "ubi_bgt0d" started, PID 36
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
d_can d_can: d_can device registered (irq=52, irq_obj=53)
mice: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=0:17:eb:50:e0:d6
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
>>>> phy_connect:bus id 0:00<<<<
CPSW phy found : id is : 0x221611
>>>>cpsw_set_phy_config <<<<
>>>>cpsw_set_phy_config: Link Status 796d <<<<
IP-Config: Complete:
device=eth0, addr=192.168.1.177, mask=255.255.255.0, gw=192.168.1.16,
host=kiwidev, domain=, nis-domain=(none),
bootserver=192.168.1.188, rootserver=192.168.1.188, rootpath=
Waiting 5sec before mounting root device...
PHY: 0:00 - Link is Up - 1000/Full
UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read 126976 bytes
UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read 126976 bytes
UBIFS: recovery needed
UBI error: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:10240, read 11 bytes
UBIFS error (pid 1): ubifs_leb_read: reading 11 bytes from LEB 8:6144 failed, error -74
VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 128 mtdblock0 (driver?)
1f01 2304 mtdblock1 (driver?)
1f02 128 mtdblock2 (driver?)
1f03 4352 mtdblock3 (driver?)
1f04 204928 mtdblock4 (driver?)
1f05 312448 mtdblock5 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
Backtrace:
[<c0045bd0>] (dump_backtrace+0x0/0x110) from [<c03491f0>] (dump_stack+0x18/0x1c)
r7:d6412000 r6:c006d1e4 r5:c002bffc r4:c049c110
[<c03491d8>] (dump_stack+0x0/0x1c) from [<c0349254>] (panic+0x60/0x17c)
[<c03491f4>] (panic+0x0/0x17c) from [<c00092b4>] (mount_block_root+0x1e0/0x220)
r3:00000000 r2:00000000 r1:d643bf78 r0:c03f15ac
[<c00090d4>] (mount_block_root+0x0/0x220) from [<c0009454>] (prepare_namespace+0x94/0x1d4)
[<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
r5:c00086b0 r4:c049b900
[<c00086b0>] (kernel_init+0x0/0x154) from [<c006d1e4>] (do_exit+0x0/0x5e4)
r5:c00086b0 r4:00000000
Hi John,
This could be tough one. Generally, I think that it is better in such case to use already booted Linux with mtd utils to mount, flash and sync the UBIFS partition, instead of flashing it from u-boot. This way you could rule out a problem due to a slight mistake in the flashing procedure.
http://www.linux-mtd.infradead.org/faq/ubifs.html#L_mount_ubifs
There should be exhaustive guide on the Internet for that.
I also think that it is way more easy to get mtd utils on this ARM platform using extended busybox, instead of cross-compiling mtd utils.
BR
Vladimir
Also I've checked this forum thread:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/211477.aspx
There it is suggested to apply this patch on the base EZSDK code:
I am personally not sure what is the status there and whether or not that is validated.
BR
Vladimir
If you are flashing from u-boot, this is likely a known problem that occurs because the UBI image has embedded pages of 0xFF's that it expects will be treated as empty. Alas, the ECC code for a page full of FFs is not the same as an erased page (also full of FFs), so when the UBI data is flushed (at unmount), the data written to the page is fine, but the ECC is all wrong. You don't get the ECC error until you try to read it, at bootup.
I patched u-boot to get around this by scanning the data page and skipping the write if it was empty (this assumes you've previously erase it, of course). It also works to use ubiformat from linux, which does something similar.