This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use DM8148 Camera Interface

Hi,

 

We want to use DM8148 to interface a monochrome CCD with 2 channel output (16 bits/per channel). The DM8148 data sheets mention the device has a camera interface but DM814x HDVPSS User's Guide doesn't say anything about the camera interface. We are not using TI's SDK and we want to access the registers directly. So we have several questions;

1) How can we use DM8148 camera interface? Where can we get the user's guide or application notes on the camera interface?

2) It seems DM8148 has only one 16-bit camera interface. Is it possible to interface 2 16-bit CCD outputs?

3) If we can't use DM8148 to interface 2 16-bit CCD outputs what other similar devices can we use? Will DM8168 work for us? 

Thank you very much!

 

Fred