Dear Experts,
I'm running a secondary bootloader system on an C6670 DSP..
Now I would like signalize if the first stage bootloader was successfully initalized or not.
As I saw in the sprugy5b.pdf in chapter 3.3.2 Ethernet-Ready Announcement Format the Vendor info contains all zeros.
My questions now are:
- Will there be a possibility to modify those zeros to have a status bit for the success of the first bootloader?
- If not can be the Filename or the Server hostname be modified?
- In which memoryarea can i find those values?
I hope you can help me with this.
Best Regards
Frank