Other Parts Discussed in Thread: AM1808
Hi,
I have a question about AM1808 Power Supply.
In datasheet(sprs653c)page.64 "4.2 Recommended Operating Conditions"
the RVDD CONDITION part is written as follow:
456 MHz versions / 375 MHz versions.
Let me confirm about what this "versions" means.
Is it device speed grade or actual operating frequency?
Do I need to supply 1.3v(NOM) to RVDD if I'm using 456MHz speed grade device
but actual operating frequency is 375MHz?
best regards,
g.f.