Other Parts Discussed in Thread: CCSTUDIO
Dear All,
I'm new user in CCS v5. I want to test my DSK6713's with CCS v5. Somebody help me to send me a example project like blinking LED use CCS v5 for DSK6713???
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CCSTUDIO
Dear All,
I'm new user in CCS v5. I want to test my DSK6713's with CCS v5. Somebody help me to send me a example project like blinking LED use CCS v5 for DSK6713???
Thanks.
Hi Taufiqqurrachman,
Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages (for processor issues). Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics (e2e.ti.com).
Please refer the below wiki page which has links to examples and downloads.
http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5
http://e2e.ti.com/group/universityprogram/educators/f/776/t/223996.aspx
Download board support files from below link.
http://c6000.spectrumdigital.com/dsk6713/
TMS320C6713 DSP Starter Kit (DSK):
http://www.ti.com/tool/tmdsdsk6713
TMS320C6000 Chip Support Library:
Hi Rajasekaran,
When I'm running 6713SDKDiag.exe to check my 6713 DSK boards, I get a error message "USB diagnostic fail" like below picture,
Please tell me how to solve that problem???
As your information, I'm used notebook Asus A42F series with Win7 64-bit OS.
Thank you very much and i'm waiting for your reply...
Hi Taufiqqurrachman,
Are you running 6713 DSK CCStudio 3 or Higher version of CCS?
Diagnostic application should work with the DSK version of Code composer studio.
Please refer the DSK 6713 FAQ & QSG.(http://c6000.spectrumdigital.com/dsk6713/)
DSK6713 Diagnostics works fine with CCS 3:
http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/248152.aspx
Suggestion:
Please run the 6713 diagnostics application in CCS 3 or DSK CCStudio 3 installed machine.
Hi Rajasekaran,
I'm running 6713 DSK use CCStudio v5 because if i use CCStudio v3 in Win7-64 bit then it is not working. So, I'm installing CCStudio v5 in my laptop.
Can the 6713 diagnostics application or DSK CCStudio v3 was running in Win7-64bit?
How if we are using CCStudio v5 to develop program for 6713 DSK as example to make a blink LED at 6713 DSK?
Please give me your suggestion.
Thank you very much and I'm waiting your reply.
TAUFIQ.
TAUFIQ: said:Can the 6713 diagnostics application or DSK CCStudio v3 was running in Win7-64bit?
Win7-64bit support was not available in CCS v3.
TAUFIQ: said:How if we are using CCStudio v5 to develop program for 6713 DSK as example to make a blink LED at 6713 DSK?
CCSv5 supports the on-board USB of the 6713DSK. You do not need any extra drivers. Select "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" as your connection type and "DSK6713" as your device.
Hi TAUFIQ,
We do not have any direct example projects for CCSv5 using DSK6713. However please follow the below steps.
1. Download & Install BSL. The BSL has sample project to Blink the LED.
BSL Installation Path: DSK6713\examples\dsk6713\bsl\led
2. Please download & install CSL.
3. Please follow the below wiki link to create a new project in CCSv5 for C6713DSK.
http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5#Creating_new_project
4. Please refer the below wiki link to Import the LED BSL project (newly created project from step 3).
http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5#Importing_sample_projects
Thanks.
Hi Rajasekaran,
I'm already trying the 6713 DSK Diagnostics at winXP SP2 using virtual machines software like VMWare and the 6713 DSK Diagnostics says pass. But I still trying to use CCStudio v5.0 as your suggestion. And I curious about it.
Thank you very much.