This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Overhead of Codec Server

Hi

I'm using DVSDK 2.0 on DM6467 EVM.

Base on sample of canny and 1080pstreaming, I integrate two codecs in my codec engine. 1 is 264 encoder (DVSDK2.0 Sample), 2nd is a simple codec which does nothing inside(test purpose only).

Test scenario: 25hz 720p

if I do my own codec and 264 encoder for each frame, after a few minutes, DSP stopped encoding. I saw dsp load = 0%.

but if I encode video each frame but call my codec every 5 frame, that's fine.

I am wondering if this is related to codec engine overhead?

but there is no problem if I use sample encodedecode loopback sample. encoder and decode is called for each frame.

Any idea on this?

Thanks.

if for each fr