Other Parts Discussed in Thread: AM3358, SYSCONFIG
Hi everyone,
my company has build two custom AM3358 boards for prototyping, one with 8bit (MT29F2G08ABAEAH4-IT:E) and other with 16bit NAND memory (MT29F2G16ABAEAWP-IT:E)
Few basic information:
- development environment is CSS v5.5, 06.00.00 SDK and XDS100 v2 JTAG, installed under Linux host
- we are using DDR3 and TPS51200DRCT device, attached to GPIO1_30 for VTT_ENA
- NAND memories are attached to GPMC_WAIT0 (R/B) for ROM boot support
- we do not need I2C, SPI, MMC and Ethernet support for uBoot
- but we need both 8bit and 16bit NAND support (uBoot and kernel)
- one of official uBoot git repositories link, for AM335X?
- the one available under PSP distribution?
- the one available under SDK, under board-support/board-port-labs/sitara-board-port-uboot