Hi,
We need to prove the functionality of the Hyperlink interface on a card which is connected to C6678.
For the example Hyperlink test from the MCSDK version 3.00.00.11, i have the following queries.
1. Though the test informs that it can run in both loopback and board to board mode, what exactly is loopback mode ? Is it a SW loopback ? And when it says as board to board, does it mean two EVM's connected by means of a Hyperlink cross over cable ?
2. A littile more infomation about the HW & SW test setup would be helpful.
3. As there are two ports of Hyperlink, how to test both the ports ?
4. Does the same example work for both loopback and board to baord mode ? If yes, then what is the modification to be made? are there any flags that need to be enabled & disabled?
Regards
Pradeep