Hi,
I am trying to get display on DVI interface in OMAP3EVM Mistral Board with DM3730 processor module by running linux-3.7 kernel image. But I am not able to get display on DVI interface. Does linux-3.7 have DVI/HDMI display driver support for OMAP3EVM DM3730 ? Am I missing anything in bootargs ?
I am passing bootargs as follows from u-boot
console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omapfb.mode=dvi:800x480MR-24@60 omapdss.def_disp=dvi init=/bin/sh vram=20M
Log Message
[ 0.000000] Linux version 3.2.0 (tharma@tharma-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #2 SMP Fri Sep 27 18:03:23 IST 2013
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omapfb.mode=dvi:800x480MR-24@60 omapdss.def_disp=dvi init=/bin/sh vram=20M
...
...
...
[ 2.020477] omapfb omapfb: no driver for display: lcd
[ 2.025970] omapfb omapfb: no driver for display: dvi
[ 2.031311] omapfb omapfb: cannot parse default modes
[ 2.060943] Console: switching to colour frame buffer device 90x35
...
...
FYI,
1. By running linux-3.7 kernel image, I am able to get display on TVOUT interface for following bootargs
console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omapdss.def_disp=tv omapfb.mode=tv:pal init=/bin/sh vram=20M
2. By running linux-2.6.37 kernel image, able to get displau on DVI interface for following bootargs
console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omapfb.mode=dvi:800x480MR-24@60 omapdss.def_disp=dvi init=/bin/sh
console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omapfb.mode=dvi:720x480@60 omapdss.def_disp=dvi init=/bin/sh
Attached file is kernel configuration (.config) file
Regards,
Tharmarajan G