Other Parts Discussed in Thread: OMAP3530, OMAP3503
Hi,
I'm trying to rebuild the linux kernel for the OMAP3530 EVM board. The document I'm using is the Aug 2008 version of OMAP3530 DVSDK Getting Started Manual.
When I run 'make menuconfig' as documented in chapter 6.2 "Rebuilding the Linux Kernel" and select 'System Type', I see a different interface as that in the manual. The interface looks like this:
ARM system type (TI OMAP) --->
TI OMAP implementations --->
---OMAP Core Type
[] OMAP730 Based System (NEW)
[] OMAP15xx Based System (New)
[] OMAP16xx Based System (New)
---OMAP Board Type
[] TI Innovator (New)
... ...
[] Generic OMAP Board
--- OMAP CPU Speed
[] OMAP clocks set by bootloader (NEW)
[] OMAP ARM 168 MHz COU (NEW)
[] OMAP ARM 150 MHz COU (NEW)
[] OMAP ARM 120 MHz COU (NEW)
[] OMAP ARM 60 MHz COU (NEW)
[] OMAP ARM 30 MHz COU (NEW)
[*] OMAP35x Family
Current choice (OMAP3530) --->
How should I select the Core type and the Board type? Although I selected OMAP3530, currently I'm getting errors like:
kernel/power/Kconfig:347: choice values currently only support a single prompt
....
warning: "___LINUX_ARM_ARCH___" is not defined.
Thanks,