Hi all,
i have got a strange phenomenon:
I use the dcantxrx.c example code to send a single message via CAN.
The CAN frame is correct. I measured it on the oscilloscope and tested the communication with an USBCAN Module. So far so good. If i activate the interrupt for INT_Line_0 (CAN device 0), i will get an interrupt (INT0ID = 0x0001). Thats because i transmitted via messageobject with the id 0x01.
After clearing the INT0ID Flag, the CANisr0 restarts. I cleared all interrupt flags but i get an infinity loop (the CANisr0 always restarts). During the CANisr0 i check the message id, which is 0x00 ???
I don't understand why the isr permanently reruns?
Do i have to clear some other interrupt flag but the can0 flags???
Do you have any idea why the isr reruns?
I would welcome your response!
Enclosed please find my register configuration!
Best regards Andreas