This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a question about Advisory 1.0.32 in AM335x.(sprz360f)
I am wondering the operation when following conditions occured simultaneously.
a) VDDA_ADC and AIN0 are connected, in AMUX5:1.
b) VSSA_ADC and AIN1 are connected, in AMUX4:1.
c) AIN0 and AIN1 are connected, in AMUX9:1.
If it occured, VDDA_ADC current flow into VSSA_ADC.
But, workaround does not say about this condition.
Q)
- Does this condition NOT occur in ADC?
- Is this condition NO problem in ADC?
Best regards, RY
Yes this is possible. However, the resistance of the internal analog switches will limit the current to a level that will not damage AM335x. That is why you only need to add external resistors which limit current to attached devices,
Regards,
Paul