This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Errata Advisory 1.0.22

Hi Champs,

I'm planning to use AM335x 1000MHz and I need to set the VDD_CORE to 1.1V (OPP100).

According to the datasheet(SPRS717J, page 88), the Standby and Deepsleep1/0 power modes require both of VDD_CORE and VDD_MPU to be set to 0.95V respectively.  However, VDD_CORE dynamic switching (OPP100 <-> OPP50) is not allowed due to the Advisory 1.0.22 in the silicon errata.

So, I'd like to make sure if I can use the AM335x Standby and Deepsleep1/0 Power Modes w/ 1.1V VDD_CORE and 0.95V VDD_MPU or not.

Best regards,
j-breeze