This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kitkat release for OMAP4 Pandaboard

Other Parts Discussed in Thread: 4460, 4430

Hi All,

I'm using the OMAP4 4460 Pandaboard ES. I would like to know,

1) Is there any chance of TI releasing Android 4.4 Kitkat for Pandaboard in the near future?

2) If yes when can we expect that?

3) If not for Pandaboard, is any other platform in OMAP4 series will be having a Kitkat release soon?

Thanks &Regards,
Geo

  • Hi Geo, 

    There are teams working on porting all the functionality for omap4 but i cannot shed any more light on that matter.

    If you are willing to test there are releases in the open communities which are classified as stable but cannot guarantee the performance that the OMAP platforms allow.

    Regards,

    Boyko

  • Hi Boyko,

    Thanks for your quick reply, It will be a great help to me if you could point out some open community sources with Android 4.4 Kitkat release for OMAP4 platform.

    Thanks and Regards,

    Geo

  • Hi Geo,

    If you are eager to try the kitkat you can go to the cyanogenmod  site, the guys there did splendid job on porting the functionality on their kernel. 

    Or you can check this article here for AOSP ( it have really good guide for beginners) :

     http://blog.sola-dolphin-1.net/archives/4575367.html

    but be aware that this branch have some graphics glitches which are removed in the other builds.

    Regards,

    Boyko

  • Hi Geo,

    I was able to build kitkat(asop) for Pandaboard ES following the steps given in the file attached below.

    I tested it on the board able to get display. 

    Hope it helps.

    Regards,

    Aashish

  • Hi Aashish,


    Thanks for the reply.

    Have you tested Wifi, BT, 1080p video, ethernet etc...??

    Regards,

    Geo

  • Hello Aashish,

    Have you been able to run it on Panda ES Rev B3 ?

    kind regards,

    Jean-Marc

  • Hi Geo,

    I have tested audio, was able to play audio samples but recording is still giving issue but I think that is because mic input is connected to FM.

    I haven't played a video yet.

    WiFi was giving some trouble still working on it but BT is up able to pair my phone to the board.

  • Hi Jean-Marc,

    My board is Panda ES Rev B1.

  • Hi Ashish,

    I have followed the steps given by you and I am able to see the android home page.

    But everything including the console is getting freezed with in one or two minutes after booting up.I tried with three different panda boards, all are behaving the same way.

    Can you suggest something about this??

    Thanks and regards,

    Geo

  • Geo,

    ##

    But everything including the console is getting freezed with in one or two minutes after booting up.I tried with three different panda boards, all are behaving the same way.

    ##

    That is coz that time there is no wake lock on system.In panda board system suspend will block the console also, so if u need to console should be on u can enable wake_lock to sytem or make change in kernel to stop suspending console.

    Regards

    Vikram

  • Thanks Vikram ,

    Anyway that is not case, because wake_lock is already enabled and i am able to navigate the mouse also

    Regards,

    Geo

  • Hi ,

    Sorry I forgot to attach the patches mentioned in the document I uploaded earlier.

    Here are the patches.

    panda_kitkat_patches.zip
  • Hi Aashish,

    I managed to get those patches from blog.sola, still the android is very unstable.

    Bluetooth is working fine. But the android and console is getting freezed randomly.

    Have you faced this issue??

    Thanks

    Geo

  • Hi Geo,

    No we are not facing any unstablity issue as of yet and we have recompiled this source and flashed it many times.

    Can you send log file?  

    Also which manifest branch have you cloned ? We are using android-4.4.2_r1 ?

  • Hi Aashish,


    i was using android-4.4_r1.1, i will try the other and will update soon

    Thanks and regards,

    Geo Joseph

  • Aashish,

    Can you please provide the two patch files in your supplied document for U-boot and the Kernel?

    uboot:    "0001-change-bootarges.patch" and kernel:    "0001-panda-jb4.2_kernel.patch"

    Thank you!

    mccabet

  • Hi All,

    I have uploaded the updated kitkat_porting_step_pandaboard.txt document in the same reply I posted earlier. 

    Manifest Branch for repo sync in new doc is android-4.4.2_r1 and also corrected few typos ( Sorry for those )

    thomas mccabe said:

    Aashish,

    Can you please provide the two patch files in your supplied document for U-boot and the Kernel?

    uboot:    "0001-change-bootarges.patch" and kernel:    "0001-panda-jb4.2_kernel.patch"

    Thank you!

    mccabet

    Hi Thomas,

    I have uploaded the zip containing this patches in earlier reply in the same post. Do check them and let me know if you have any other issue.

  • Hi Aashish,

    I tried with android-4.4.2_r1, still its having the same problems.

    Could you please share the working binaries??

    Thanks and Regards,

    Geo

  • Hi Geo,

    are you sure console stops while you can still move the mouse pointer. We had the wake_lock issue but we got rid of it as vikram suggested.

    And have u tried prebuilt images from linaro release of kitkat for panda board. 

    http://releases.linaro.org/14.03/android/panda/

  • Hi Aashish,

    For me everything works fine till i click any app in android and the system goes to freeze, some times its simply freezing. And wake_lock is on also.

    The 14.03 linaro prebuilts are working fine for me .

    Thanks and Regards

    Geo

  • Hi Geo,

    I actually played around with some apps myself media player etc didn't get this issue. Can you please upload bootlogs file and logcat output . It will help in debugging whats going on.

  • Hi Aashish,


    Please see the attached log file.

    The console got stuck when i clicked on settings of app menu

    Regards,

    Geo

  • Hi Aashish,

    Thanks for the support, it was a hardware issue.

    I tested on a new Panda ES board, its working.

    Wifi is showing a crash message but working. Default browser is having issues. 

    Also for Bluetooth not all profiles are there.

    1080p video support is not there, is there any way to bring Ducati support??

    I haven't tested Camera also.

    Regards,

    Geo

  • Hi Geo,

    Even we think its a hardware issue becuase we tested the same images on pandaboard A6 and we are getting similar issues of freezing at random points. We think its the RAM issue but we are still trying to debug the actual cause and get patch to fix it.

    We have not explored the bluetooth module in depth. Can you please share which bluetooth profiles are supported. Also have you  seen Handsfree mode implementation for HFP anywhere. We trying to implement that functionality on android since by default it has only audio gateway mode implementation. If you have come across some links for implementing the same can you please share them or point us in the right direction.

    Thanks in advance

  • Hi Jeo,


    Can u tell me which pandaboard revision u were using in which u are facing android freezing issue.And what's ur new pandaboard revision which is working with same images.

    Thanks

    Vikram

  • Hi Ashish ,

    We haven't tried any thing related to Handsfree mode. Also A2DP was not working with this.

    Also freezing issue was cropping up at times , so moved to Linaro port.

    Thanks

    Geo

  • Hi,

    I was facing the android freezing issue with PANDA board revisions A ,A3.

    But it was  fine with PANDABOARD RevB2 ES. But only once or twice this board also got freezing issue.

    I believe the freezing is caused by the PVR chip difference in these boards.

    Thanks,

    Geo

  • HI Geo,

    Thanks for your reply.

    As we mentioned earlier we switched to Pandaboard A6 and facing the same freezing issue with both linaro(14.05) and asop images and trying to get the root of the issue so that we can make the necessary changes. But everything we tried so far didn't help.

    Which Pandaboard revision were you using ?

    And did linaro 14.03 images worked for that board ? Or you tried those on Pandaboard ES ?

    Were you able to debug the hardware issue with that board ?

  • Hi Ashish,

    As I said in the earlier post sola sources are working on PANDABOARD RevB2 ES .

    The linaro port i tried was 13.11 and it was working fine with all these boards means (A1.A3,B2 ES) and its haven't shown any freezing .

    I believe there is difference between Rev A and Rev B (ES) is the chip it used means 4430 and 4460 , which basically has different PVR inside the architecture. So PVR modules for 4430 might work on 4460 but vice versa might not work. 

    Thanks

    Geo

  • Thanks Geo for ur info.


    Thanks

    Vikram

  • Hi,

    Do anyone got successful in bringing up Ducati on Kitkat..?

    If so please share me the details

    Thanks and Regards

    Geo

  • Does this work on Panda A4 board?

    I also tried using the pre-built Linaro Kitkat binaries, but the video does not boot up. Only able to access the shell? Is there something I need to do?

  • Hi Anthony,


    So far we have tried it on Pandaboard ES B2 and B3 revision.

    On B3 revision with some changes in xloader (RAM related ) since RAM on B3 is different.

    Other than that it works fine for us we are getting display on HDMI also tried with external LCD.

    We also tried on Panda A6 board but it was highly unstable. We made some RAM related changes then it would boot but then it will freeze if we run any application.

  • Hi Aashish Patel,

     I am building android kitkat 4.4.2 for PandaBoard ES REV B1, with the procedure give by you.

    I am unable to build source, it is giving some errors.

    I was not able to figure out the error.  I am attaching the build log.


    Kindly help me,


    Thanks in advance,

    Santosh

    0820.buildlog.txt