Hello,
I implemented IDLE mode 3 with PLL disabled according to the instructions giving in C5502 data manual SPRS166K. I used WDT to wake up the system after 1000ms. Every thing seems to work fine when I am using JTAG emulator however when I load the code into flash then system does not go to low power mode. I could not figure out what is making the system behave that way when i am running code from the flash. Any idea or suggestions are welcome.
Thanks,
-Kashif