Other Parts Discussed in Thread: OMAPL138, AM1808
Hi
I've custom OMAPl138 board based on omap LCDK board. when i boot the board first time with the following files from SD card /board-support/prebuilt-images/ u-boot-lcdk.bin, u-boot-lcdk_ais.bin, uImage successfully it got boot.
But suddenly its getting restarting and its not booting again it failing in u-boot. log is here. and it have NAND memory.
stop stop5 stop51 stop53 stop54 stop56*** Warning - bad CRC, using default environment
stop57 stop58 stop59 stop60 stop6In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
NAND: eee!!!
vvvvvvvvv!!!
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
NAND bus width 16 instead 16 bit
gggggg!!!
hhhh!!!
512 MiB
MMC: vinothrajdavinci: 0
stop stop5 stop51 stop53 stop54 stop56*** Warning - bad CRC, using default environment
stop57 stop58 stop59 stop60 stop6In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
NAND: eee!!!
vvvvvvvvv!!!
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
NAND bus width 16 instead 16 bit
gggggg!!!
hhhh!!!
512 MiB
MMC: vinothrajdavinci: 0
stop stop5 stop51 stop53 stop54 stop56*** Warning - bad CRC, using default environment
This is the log i'm getting again again.
How can i resolve it. ?