Other Parts Discussed in Thread: OMAP-L138
- DDR Configuration
- OMAP-L138/Common/src/device.c: Modify the parameters passed to the function DEVICE_ExternalMemInit to match the DDR timing requirements for the custom board
- UART Settings
- OMAP-L138/Common/include/device_uart.h: Modify the #define DEVICE_UART_PERIPHNUM to set which UART is connected to the host PC.
- Note that flow control is not used, so only the RX and TX lines need to be connected for boot and flashing purposes.
- SPI Settings
- OMAP-L138/Common/include/device_spi.h: Modify the global macros to select the appropriate peripheral and chip select numbers.
- OMAP-L138/Common/src/device_spi.c: Modify the flash organization in DEVICE_SPI_MEM_params.
- The SPI flash on the EVM does not need to be unlocked in order to erase or write. Some SPI flashes may need to set the BL bits before writing. Check the device datasheet to see if this step needs to be added to the initialization.
- NAND Settings
- OMAP-L138/Common/include/device_async_mem.h: Modify the #define DEVICE_ASYNC_MEM_NANDBOOT_BUSWIDTH to match the bus width of your NAND
- PLL Settings (for non 24 MHz input clocks)
- OMAP-L138/Common/src/device.c: Modify the parameters passed into the function DEVICE_PLL0Init and DEVICE_PLL1Init to set the proper PLL output frequencies
- OMAP-L138/Common/src/device_uart.c: Modify the 'divider' field in DEVICE_UART_config to achieve 115200 baud rate
How can i modify Settings where
- NAND is 8bit
- PPL is 24Mhz
- UART is connected through UART(2)
I dont understand the DDR configuration