Dear all,
We found the HDMI output is not the same with original source. We know we can set register 0x46c00524(VID_ACEN) to adjust HDMI output. But the original source can not meet the measured signal. For example, when we set this register to 0x0, the source gray color range from 0~17 is measured to 1, range from 235~255 is measured to 254. When set this register to 0x2, the source gray color(range from 0~17 is measured to 16, range from 235~255 is measured to 234. Could we let the HDMI output signal be the same with the original signal? And any other registers can be set to do this? Thanks a lot.
Sincerely,
James