Hi, could you help me, please, with my misunderstanding?
I load simple UART example (*.dat) into NOR flash. Then I boot DSP from this flash. Everything works correctly (rev.2).
Then I try to boot via IBL NOR boot. But there is only "ibl: booting from nor" in hypertherminal. It means that default project was loaded and I would like to load my UART example, which was loaded into the same nor flash.
Is it possible to load from IBL first and then ftom SPI with my example? This way of booting I need for rev.1.
Thank you in advance, Yuliya.