This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Arago Linux in Omap-l138 doesn't boot

Other Parts Discussed in Thread: DA8XX, OMAPL138

Hi everyone,

I have a problem with the board omap-l138. Since a few days ago, when i booted the board following the Quick Start Guide, Arago Linux started without problems.

This morning Arago Linux didn't boot. I try to copy the boot messages here:

NAND:  512 MiB
MMC:   davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
Net:   Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot:  0
reading boot.scr

** Unable to read "boot.scr" from mmc 0:1 **
reading uImage

2040348 bytes read
## Booting kernel from Legacy Image at c0700000 ...
   Image Name:   Linux-3.1.10
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2040284 Bytes = 1.9 MiB
   Load Address: c0008000
   Entry Point:  c0008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 3.1.10 (root@VPC-U1104) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #7 PREEMPT Fri May 11 11:15:57 CDT 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 LCDK
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 32512
Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125856k/125856k available, 5216k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xff000000 - 0xffe00000   (  14 MB)
    vmalloc : 0xc8800000 - 0xfea00000   ( 866 MB)
    lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .text : 0xc0008000 - 0xc0396218   (3641 kB)
      .init : 0xc0397000 - 0xc03ba000   ( 140 kB)
      .data : 0xc03ba000 - 0xc03db160   ( 133 kB)
       .bss : 0xc03db184 - 0xc03f4c1c   ( 103 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 227.32 BogoMIPS (lpj=1136640)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
NET: Registered protocol family 16
EMAC: MII PHY configured
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
Switched to NOHz mode on CPU #0
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
msgmni has been set to 245
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver unknown
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb1: New USB device found, idVendor=1d6b, idProduct=0001
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: DA8xx OHCI
usb usb1: Manufacturer: Linux 3.1.10 ohci_hcd
usb usb1: SerialNumber: ohci.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
  #0: DA850/OMAP-L138 EVM
TCP cubic registered
NET: Registered protocol family 17
davinci_emac davinci_emac.1: using random MAC addr: 2e:b5:0e:18:8d:eb
mmc0: new SDHC card at address 1234
console [netcon0] enabled
netconsole: network logging started
mmcblk0: mmc0:1234 SA04G 3.63 GiB
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
 mmcblk0: p1 p2 p3 < p5 >
ata1: SATA link down (SStatus 0 SControl 300)
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
Freeing init memory: 140K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udevd (946): /proc/946/oom_adj is deprecated, please use /proc/946/oom_score_adj instead.
Remounting root file system...
Caching udev devnodes
Populating dev cacheFAT-fs (mmcblk0p3): invalid media value (0x1f)
FAT-fs (mmcblk0p3): Can't find a valid FAT filesystem
mv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:07, id=7c0f1)
ADDRCONF(NETDEV_UP): eth0: link is not ready
eth0      no wireless extensions.

udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
Tue Apr 10 18:57:00 UTC 2012

HERE the boot process stops indefinitely

 


Could anyone help me? I'm really stuck!