Hello, everyone.
I'm working with the Sitara AM335x SK, and with the Linux SDK 05.05.00.00.
I'm using a Linux host PC with Ubuntu 11.14 installed, and the SDK installed quite successfully (used the USB cable provided to connect the SK, which had the SD card inserted, to the PC), along with CCS v5 too.
I'm now trying to run the setup.sh script so as to configure my development environment, as per the instructions of the SDG (the .pdf file found in the SD card itself). I edited the file that checked for the version of Ubuntu to be 10.04, and commented out the lines that caused the program to abort. However, in the second step, when checking for installed packages, none are found and the program aborts. The SDG, on the other hand, states that all packages not installed will be installed at this step.
Am I missing something here? Is any other script to be changed so as to enable a successful completion of the setup process?
Also, as an aside, is a router/switch necessary to connect the PC and the SK? If they are to be connected only in a local network, will a simple cable not do? Or is emphasis to be laid on their connection to the internet as well?
Will be grateful for any help,
Thanks,
Madhusudan