Hi,
I used the ti-sdk-am335x-evm-07.00.00.00.
Now I can run Graphics SDK OpenGL ES2.0 Demos(the LCD displayed the demos correctly),but there are some mistakes as blew:
root@am335x-evm:/opt/gfxsdkdemos/ogles2# ./OGLES2MagicLantern PVR: Hint: Setting WindowSystem to libpvrPVR2D_FRONTWSEGL.so PVR:(Error): PVRSRVMetricsTimeNow: using (potentially) low resolution timer [97, /pvr_metrics.c] PVR: PVR: Memory Stats PVR: ------------ PVR: PVR: High Water Mark = 4200 bytes PVR: PVR: 4200 bytes still allocated in 1 allocations PVR: PVR: 1 - 4200 bytes at 0x3b93c8 - eurasiacon/imgegl/tls.c:31 PVR: PVR:(Warning): PVR2DEnumerateDevices: display device name too long, truncating [142, /pvr2dinit.c] PVR: PVR: Memory Stats PVR: ------------ PVR: PVR: High Water Mark = 4200 bytes PVR: PVR: 4200 bytes still allocated in 1 allocations PVR: PVR: 1 - 4200 bytes at 0x3b93c8 - eurasiacon/imgegl/tls.c:31 PVR: PVRShell: EGL 1.4 initialized PVR:(Error): OSIsProcessPrivileged: not implemented, default returns false [562, /osfunc_um.c] PVR:(Warning): Running StartUpMemSpeedTest. High memory watermark will be ruined. Disable using apphint EnableMemorySpeedTest [45, /metrics.c] PVR: Bytes : 512 1024 2048 4096 8192 16384 32768 65536 131072 PVR: ---------------|-------|-------|-------|-------|-------|-------|-------|-------| PVR: H -> VB: 221.69 529.81 575.31 512.44 545.41 613.29 593.52 612.32 608.41 PVR: H -> H: 605.01 660.40 669.83 518.82 537.01 589.79 590.60 579.06 541.92 PVR:(Error): PrepareTextureUpload: Can't do sub tile twiddling to unaligned surface/stride! [1619, /sgxtransfer_queue.c] PVR:(Warning): SGXQueueTransfer: all paths failed in TQ, returning error (this is not a bug) [9679, /sgxtransfer_queue.c] PVR:(Warning): HWTQTextureUpload: Failed to load texture image (error=19). Falling back to SW [531, /texdata.c] PVR:(Error): SGXQueueTransfer: all paths failed [9683, /sgxtransfer_queue.c] PVR:(Warning): HWTQTextureUpload: Failed to load texture image (error=3). Falling back to SW [531, /texdata.c] PVR:(Warning): PrepareToDraw: Creating ZS buffer for SPM [1113, /sgxif.c] PVR:(Warning): PB Watermark Info - Alloc: 0x259 , Free: 0x584 [471, /sgxrender_targets.c] PVR:(Warning): RTDataset SPM Details: OUTOFMEM: 0x2, SPMRenders: 0x0 [479, /sgxrender_targets.c]
I want to know that is there something wrong?