Hi,
I had a test program to check for DIV0 in my c++ program below:
extern __cregister volatile unsigned int FAUCR;
void testDIV0(void)
{
double a = 1, b = 1, c = 0;
c = 0;
b = 1 / c;
printf("\nFAUCR = 0x%x", FAUCR);
}
I expect to see DIV0 in FAUCR set, but the output I get is:
FAUCR = 0x800000
Why is FAUCR not showing DIV0? How do I perform tests to enable FAUCR to flag out the exceptions such as
underflow or overflow, the rounding mode, NaNs, denormalized numbers, and inexact results? Thanks!