This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713 MCBSP SPI READ DATA ERROR

Hi, dear all.

   I need to communicate with a  FLASH, so I set MCBSP as  SPI master, 8bit, MSB.

   I am sure SPI write and read alone (before reading need to write a dummy number) will be ok.

    However, practical applications, often need to wirte and then read followed, for example, reading a

register from the slave :we need to  write address, write the control word, and then  read. There have a problem! ! !

For example:

SPI_Send_Bytet (Reg_H); // write  registers high 8BIT address

SPI_Send_Byte (Reg_L); // write  low 8BIT address

SPI_Send_Byte (FDM2 | RWB_READ | (s * 0x20 + 0x08)); // write control byte via SPI

SPI_Send_Byte (0); // write dummy 
X_H = SPI_Read_Byte (); // read 16BIT register high 8BIT

SPI_Send_Byte (0); // write dummy

X_L = SPI_Read_Byte (); // read the low 8BIT of 16BIT register /////////////////////////////////// ////////////////////////////////////////////////// //////////////////////////////

There are five groups 8bit clock sequence in the course of operation.

The first three groups 8bit correspond to the host write 3 bytes, then the last two 8bit  for the host reading 2 bytes

I used an oscilloscope to observe, mcbsp data transmission pin, the data are OK.

But mcbsp data receive pins, within this 5 group 8bit clock sequence,

I know that , the 4th,and 5th clock group corresponding  data is I need.

However, I read the data use above, I can not get data I need ,every time , it maybe the 1st 2nd data, or so .

it will be appreciate if  somebody can tell me ,how to get the right data?